Hello,
The AD9225 is one of the 1st generation 12-bit CMOS ADC's released in the late 1990's. As you state, it does not include a PWDN pin which exists on future generations of this product family. No additional delay is required (other than…
Hello,
The AD9225 is one of the 1st generation 12-bit CMOS ADC's released in the late 1990's. As you state, it does not include a PWDN pin which exists on future generations of this product family. No additional delay is required (other than…
Hi Doug:
I was able to validate the SPI write commands, using the register 0x08 for powerdown (drop in current sourced). I also checked the Test mode register 0x0D, and I was able to test the midscale short, positive FS and negative FS output test mode…
Hi Meir,
You may want to check the ADI website and do a parametric search to filter the product display base form your recommended specification.
www.analog.com/.../10169
Here are some ADCs that might help you start with, kindly see attched file.
…AD693 |
AD5410 |
AD5412 |
AD5420 |
AD5422 |
AD5735 |
AD5755 |
AD5755-1 |
AD5737 |
AD5757 |
AD5421 |
AD421 |
AD5758 |
AD7569 |
AD7669 |
AD7868 |
AD7869 |
AD5593R |
AD5592R |
AD5940 |
AD5941 |
AD7293 |
AD7294-2 |
AD7292 |
AD5590 |
AD7294 |
L… |
Hi scottbehr,
Choosing a high sample rate converter will definitely aide in reducing the cost and complexity of the anti-aliasing filter (AAF). Next, if possible, choose a 20MHz BW to be within baseband at Fs/4 or greater, this will push the harmonics…
Hi 6j5,
The parallel equivalent in AN-742 is shown because we are looking at the input differential into the ADC. I also think you are referring to an older revision of this app note. So I attached the latest.
In all the ADC impedance tables that are…
Hi,
I'm studying how to properly design the ADC input of AD9258 and AD9268.
I downloaded S-parameters files available on the website and I would like to understand why those 2 ADCs show a different type of impedance: one rather capacitive, and the…
高性能魔术转换器(ADC)“前端”的输入配置设计对达到要求的系统性能至关重要 。优化总体设计取决于很多因素 ,包括应用性质、系统组成和ADC的结构。以下的问答主要节绍了使用放大器和变压器影响ADC前端设计的一些重要的实际考虑。
问:放大器和变压器根本区别是什么?
答:放大器是有源器件,而变压器是无源器件。放大器和其它所有的有源器件一样,消耗功率并且产生噪声;变压器不消耗功率并且产生的噪声可以忽略不计。两者都涉及到动态效应问题。
问:为什么选择放大器?
答:放大器的性能限制比变压器少…
关于宽带ADC前端设计考虑ΙΙ:用放大器还是用变压器驱动ADC?
By Rob Reeder [rob.reeder@analog.com]
Jim Caserta [jim.caserta@analog.com]
高性能模数转换器(ADC)“前端”的输入配置设计对达到要求的系统性能至关重要 。优化总体设计取决于很多因素 ,包括应用性质、系统组成和ADC的结构。以下的问答主要节绍了使用放大器和变压器影响ADC前端设计的一些重要的实际考虑。
问:放大器和变压器根本区别是什么?
答:放大器是有源器件…