FAQ
I want to getting a voltage level from AD9236. But when I test AD9236 (ADC) It is difficult to anlayze a signal with low frequency. As this reason, I can't get a DC(direct current) voltage value.
ADC is always used for fluctuating signal?
As far as…
yes, it is all clearly explained in the datasheet. see ANALOG INPUT AND REFERENCE OVERVIEW section
I'm designing a DAQ system with AD9236, and with 1V reference voltage. It seems it has internal reference, the data sheet only specified the typical and max error at 25 ℃, and apparently this is not the situation when the AD is running at full speed…
Now, I am planning Implementation of AD9236(ADC) on the ZYNQ Custom board.
OS on the Board is Petalinux.
Firstly, I make signal (1Mhz) PS and then connect it to ADC. Then I added IP-Core(AXI-GPIO) with 12bits as GPIO-Width. But when I checked on the…
I want to getting a voltage level from AD9236. But when I test AD9236 (ADC) It is difficult to anlayze a signal with low frequency. As this reason, I can't get a DC(direct current) voltage value.
ADC is always used for fluctuating signal?
As far…
Hi rf_engineer_5,
The AD9251 ADC diff input is a switched capacitor arrangement:
According to AN-742 Application Note, the ADC input impedance will have Real and Imaginary components that vary between the Track to Hold mode. From this application note…
My ADC is AD9236, when using 1.0V external reference, the typical input span is 2Vp-p per the data sheet.