• AD9233: 0x18 register setting the input range

    Regarding the 0x18 register shown in page 26 of the datasheet, the internal
    reference of AD9233 is 0.5V. There is no description of the internal reference
    resistor divider inside the chip in the datasheet. Would you please clarify the
    function…

  • AD9233待机问题

    请问一下控制ad9233转换和停止转换是只能通过直接控制时钟通断来实现吗?如果采用晶振作为时钟源,又如何控制AD采样呢?采用PWDN引脚可不可以控制?

  • AD9233待机问题

    请问ADI工程师 AD9233在工作时停止时钟输入的话,是不是只是停止数据转换呢,与掉电模式功耗差别是怎样的呢?

  • AD9233  CML电压设置

    你好,我公司产品上用的AD9233,发现有些产品上的AD9233 CML引脚输出的电压不太一样,大概在电压范围在0.93V 到0.96V之间;(AVDD是1.8V的)我看到AD9233的手册上说,CML电压设置在0.55*AVDD是最好的;但我们做了这么多,从没发现达到0.55*AVDD(0.99V);所以就请教你们,这个CML引脚电压是怎么调压的?

  • AD9233 oscillation

    Hello, we are developing a new acquisition unit with AD9233, we design the  antialea and the FDA chain to drive the ADC. 

    We product more or less 20 sample (ten layers board with Zynq ecc) but in only one sample we found a 27MHz  oscillation (500mVpp)  from…

  • FPGA控制AD9233

    你好,ADI工程师,我是做超声仪器的,在超声信号采集端,想选用AFE的芯片,但都是多通道的,我只需要单通道就够了,现在看到AD9233性价比比较符合我们要求;然后,我做的数据采集方案是 FPGA 来控制AD9233做高速采集;通过FPGA的FIFO缓存传给MCU;发现AD9233没有FPGA控制的实验室电路;能否推荐些FPGA控制AD9233采样的资料给我;主要不明白:AD9233的时钟不是从FPGA发出;计划选用AD951x系列芯片产生时钟;这情况下FPGA可以设置AD9233的采样速率吗;通过什么方法…

  • 怎样启动和停止AD9233采样

    你好,ADI工程师;请教用FPGA控制AD9233,时钟芯片用AD9515;想请教的问题是:外部数字触发信号输入到FPGA,识别后,启动AD采样;这个启动AD9233是怎么操作的;是控制AD9515输出时钟吗?如果启动采样后,在采样点数到后;怎么停止采样,是不是禁止AD9515的时钟输出?谢谢!

  • AD9233数字地,模拟地需要隔离吗?

    你好,ADI工程师们,请教高速AD采样板卡怎么设计数字地和模拟地?我用的采样芯片是AD9233BCPZ-105,采样频率最高到105M,时钟芯片用的是AD9516-4;PCB为四层板,顶层走高速信号,第二层设置为地层,第三层为电源层,地层走低速信号;PCB布局完后,模拟信号输入通道只占用一小部分;附件是PCB的布局图;现在请教电路板数字地和模拟地需要分割吗?然后在AD9233附近通过0欧姆电阻单点连接?如果不需要分割,是不是在PCB第二层设置为统一的地层,以保持完整?哪种效果更好?希望得到贵公司的指点…

  • AD9233转换 结果;需要补偿一个偏置量吗?

    你好,ADI工程师;请教;AD9233转换 结果;需要补偿一个偏置量吗?AD9233设置是:采用内部偏置1V;采样时钟50M;二进制输出格式;

    当我输入100K正弦信号;峰峰值 2Vpp;  采集到的数据波形(用的QUARTUS Signal tap查看的);在没有补偿偏置时,波形溢出;当补偿一个  0x80 (12'h80);波形就回到中间点;就是一个完整的正弦波!请教这个补偿是必须要添加的吗?