• AD9211ad9230_relationship

    I want the layout information about AD9211 EVAL board.

     

    the AD9211 is the 10-bit version of the Ad9230.  these are pin compatible and
    share the same eval board so the Ad9230 or AD9230-11 eval board info would be
    better suited. 
  • AD9230

    I am looking at worse case timing for a design that I am doing at the moment using the AD0230 ADC. A typical value is provided on the data sheet, Table 4, for the propagation delay from CLK to DCO, tCPD, but no maximum time is given. Is this figure available…

  • AD9230 differential input curiosity

    Hi All,

    On page 21 of the AD9230 data sheet : http://www.analog.com/static/imported-files/data_sheets/AD9230.pdf

    We read about the shunt capacitor used at the data + and - inputs of the AD9230.

    All the termination schemes I've read about use a R value…

  • AD9515

    Hi, I want to use AD9515 as clock driver to AD9230. According to the spec of AD9515, the low level of clock output is 3.3-1.76=1.54V for LVPECL and 1.0V for LVDS. However, AD9230 recognizes clock as low only when the voltage is below 0.8V. I dont understand…

  • RE: AD9144 PRBS parallel functions?

    Dear, Lars,

    So according to your algorithm, scheme for generation of pn7 function should be such:

    Is it correct scheme? It will be compatible with the AD9144?

    But even if I will use the eight registers ([0]...[7]) and the proposed algorithm, I still…

  • AD9230 output unexpected result

    hi,

       I am using the high speed ADC of AD9230 for DPD feedback channel.

      The sample rate was 120MSPS, analog input common mode voltage was 1.46V; and Rbias pin was 0.5V; SDR mode, two complement output.

      In order to verify the ADC's noise floor,…

  • 关于AD9230的使用

    各位好,

    最近要做的一个接收机中频采样要用到AD9230这款芯片,

    之前一直用AD6645,不知道AD9230在使用上有什么要特别注意的地方吗?

    如果有设计过ad9230电路的朋友能否给提供以下建议,多谢!

  • RE: Schematic for AD9230 Eval

    Hi Samer,

    I'm attaching the schematic that matches your AD9230 Eval Brd Photo.

    Best Regards,

    Tony M

  • AD9655 interfacing and external triggering


    For a past project I used an AD9230 evaluation board with the HSC-ADC-EVALC interface board.

    Now I'm moving to a 2-channel design and I was thinking to use the AD9655.

    Is is possible to use it with the same interface board?

    Since I needed external…

  • Is there a INL diagram available for the AD9634?

    Since we would like to average repetetive signals we are interested in the Integrated NonLinearity of the AD9634. Is there a diagram available like for the AD9230?

    From the multistage architecture, is it quite repetitive like that of the AD9230 for 2…