• AD9214使用求助

    调试AD9214,已经烧了1打,感觉自己不再会用AD了

    1.为什么将AD9214输入AIN和/AIN 同时接地会把AD损坏?

    2.按照Datasheet做的原理图,在调试输入网络的时候经常烧坏AD,请问输入端有哪些必须注意的地方?

  • Minimum Frequency of Inputs for AD9214 and AD6644

      Good morning.  I have a customer inquiring as to how low the freqeuncy of a signal can be to drive the analog inputs of the AD9214-105 and the AD6644-65.  He needs to be able to accommodate some signals that will be in the range from 50KHz - 100KHz.

  • RE: About ADC

    Hi Tom,

    I reviewed your AD8138 and AD9214 schematic blocks. I do not currently have access to a viewer for your Altium Designer file. Maybe you could export to a pdf or take a screen image capture? Are you experiencing a specific issue with your circuit…

  • RE: Question about High speed ADC

    Hi,

    I've got this chip AD9211-200 with AD8138 as the ADC driver,actually AD8138 maybe the 2nd choice chip on your recommended ADC driver for AD9211 list,I think it's all OK.

    I found AD9211 is a internal bias ADC,and I need the ADC to be good…

  • AD9218: using two AD9216 - Duty Cycle Stabilizer - running the two clocks 180 degree

    I want to know is whether (and why) it would cause problems if I
    run the *two* AD9216 channels with 50% duty cycle clocks 180 degrees
    apart, for interleaving purposes.

    The relevant part of the datasheet is page 22 as follows:
    The AD9216…
  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…