在datasheet中 有描述到:REFTF and REFBF will drive the ADC conversion core and establish its maximum and minimum span. 他们的最大最小值是如何确定的,和REF电压之间有什么样的关系?在图表19 20 21三张图中,找不到他们之间的关系.知道的朋友指教下
在datasheet中 有描述到:REFTF and REFBF will drive the ADC conversion core and establish its maximum and minimum span. 他们的最大最小值是如何确定的,和REF电压之间有什么样的关系?在图表19 20 21三张图中,找不到他们之间的关系.知道的朋友指教下
Hello,
The customer had designed their circuit same as Fig. 20 (internal reference set for a 1V span),
but there are no output voltages on VREF(0.5V), REFTF(1.25V), REFBF(1.75V).
I would appreciate if you have any idea that should be checked.
…For the AD9203, how long does the part require to enter and leave standby mode?
Hi,
The AD9200 is a legacy product released 20+yrs ago before we started routinely including package thermal characteristics. My best recommendation to approximate ThetaJA on the AD9200 would be to compare it to a newer product that shares similar Package…
AD8138 -- 使用过的第一款ADI的运算放大器!
应用:使用在 CMMB数字电视接收机中。
用途:作为AD9203的单端转差分的输入buffer,把单端的低中频IQ信号变为差分。同时提供适合的直流偏置给AD9203。
特点:320M的高带宽以及 5 nV/√Hz的噪声参数完全胜任此工作,同时具有Vcom引脚,方便的设置共模电压。
I think most of the confusion is that AD9203 J3 provides the global clock ( device clock in JESD204 terms) and AD7-V2 J3 provides the transceiver reference clock to the evaluation design.
If you can somehow take the AD9208 J3 clock and connect it to…
Hi,
I got answers about this issue from ADI Korea.
Please refer below.
line #1 : AD9203 ( Part number )
ine #2 : ARU #YYWW ( Part number , # : Leadfree, YYWW : Datecode )
ine #3 : ASSEMBLY LOT NUMBER
I hope this help.
Regards,
Se-woon…