Hello,
Assumed that his has been answered offline. Please let us know if this is not the case.
Hello,
Assumed that his has been answered offline. Please let us know if this is not the case.
I have a similar question about AD9175 and AD9176. I can,t find differences.
thank you
但是我看到绝大部分的手册并没有提及到这个参数。比如说AD9175,AD9208。并且有些提及到这两个参数的数据手册,它也只有一个PSRR参数,并没有PSMR参数。
Can you check your ZC706 power supply, awhile ago I used one that shipped with a ZC702 and I also had strange JESD errors.
Your link stays in CGS, or occasionally moves to DATA but then moves back to CGS due to lane errors.
This is unexpected and with…
Hi N.Kokubo,
Mode 3 has a single channel per link. Each channel is IQ. The link has M=2, meaning there are two streams, one for I and one for Q (M0Sx and M1Sx below).
Yes, you could split I into DAC0 and Q into DAC1, using the Modulator Switch (a mux…
Whether AD9174 is pin compatible with AD9172, AD9173, AD9175 and AD9176. Can a common board layout be maintained to support all the chips.
Hi Dordije,
Certainly not the intended behavior... but is a known issue on an earlier Silicon revision. The R4a silicon has this resolved:
AD9171/2/3 were released on R2 silicon
AD9174/5/6 were released on R4a silicon
A later PCN has up-rev'd the AD9171…
When I was reading the ADI article "Optimizing the Power System of Signal Link-Part 2: High Speed Data Converter", I found that the PSMR and PSRR parameters used in the content were not mentioned in the datesheet of the relevant data converter. What I…