Demonstration of Analog Devices (ADI) CN0511 a Raspberry PI Signal Generator that uses the AD9166 Vector signal Generator (DAC/DDS) to generate sinewave tones from DC – 6 GHz.
Demonstration of Analog Devices (ADI) CN0511 a Raspberry PI Signal Generator that uses the AD9166 Vector signal Generator (DAC/DDS) to generate sinewave tones from DC – 6 GHz.
hi, AD9162 can't support down to DC directly. however, we have another product AD9166(https://www.analog.com/en/products/ad9166.html) that can support down to DC with single-ended output.
AD9166 = AD916x DAC + AMP. the circuits between DAC and AMO…
CW 7.5 GHz output can be obtained with NCO only mode, either with FIR85 enabled or in mix mode. DDR(FIR85) will be easier to filter but it will consume more power. Due to higher roll off from AD9164 we recommend using AD9166 for 7.5 GHz operation
6GHz…
Hi Kiran,
Thank you for your interest. Yes, you could use the AD916x to the same effect. it supports iBW up to 2.25GHz. I would suggest to set it in either mix-mode (green, below) or 2xNRZ (red).
The explanations in the AD9162 and AD9166 datasheets are…
Hello,
We plan to use AD9164 in our product, but in kernel driver it shows only AD9162, and says that AD9166 is also a compatible driver.
Can I assume that AD9164 is also compatible ? According to datasheet all the 3 devices us compatible (that's why…
Hi,
Does AD9166/AD9162/AD9172 FMC Evaluation cards has ZCU102 Motherboard reference designs,
As per my search i am unable to findout. Please give me the link if anyone finds.
Thanks In advance
Hi Taiki,
Thanks for reaching out. Below are my answers to your questions:
I am having difficulty building iio-oscilloscope from source on a raspberry pi 4 with the 64 bit OS. Other builds on the 32 bit OS and Ubuntu have always worked fine. The closing stdout message is:
-- Generating done
CMake Generate step failed. Build files…
10 月份全新中文资料上线!各位筒子们还在等啥呢?
系统方案精选 APM
在线研讨会
视频 VIDEO
ADRV9009-ZU11EG支持大规模MIMO相控阵系统的RF SOM