2.1 GHz instantaneous bandwidth is beyond the ability of the AD9161. You could use two AD9161s as an I/Q DAC pair and drive a quadrature modulator with a complex IF modulation.
Hi all,
It is mentioned in the AD9161 datasheet that AD9161 can support up to 7.5GHz RF in Mix-Mode,but now the output signal can only access 6GHz in Mix-Mode(0x152 bit[1:0] is 0b01).There is too little mention of Mix-Mode in the document, how can I use…
It is mentioned in the AD9161 datasheet that AD9161 can support up to 7.5GHz RF in Mix-Mode,but now the output signal can only access 6GHz in Mix-Mode(0x152 bit[1:0] is 0b01).There is too little mention of Mix-Mode in the document, how can I use it?
Is there an FPGA design example available for the AD9163 (or AD9161, AD9162, or AD9164)?
FPGA: XILINX KINTEX-7
DAC: AD9161BBCZ (setings: L=1, M=2, F=4, S=1, JESD lane rate 7.2Gbps)
Clock: AD9508
Clock settings: 180MHz fpga GTX, 2.8125MHz FPGA sysref, 2.8125MHz AD9161
Descriptions:
1 Lane JESD204B was used to communicate with AD9161. KINTEX…
Hi
AD9161/9162 data sheet on Page 80 mentions "If the AD9161/AD9162 are programmed for an IOUTFS = 40 mA, its ideal peak ac current is 20 mA and its maximum power, delivered to the equivalent load, is 10 × (RINT/(RINT + RLOAD) = 8 mW (that is, P =…
Hello
I want to use AD9161 and I am very low on FPGA and clock resources, so I want to know if my setup is possible.
My REF clock is 3840 MHz. I don't want to use internal PLL due to phase noise degradation.
I would like to generate a CW signal…
HELLO
I have a question about how to use the AD9161
It is about the solution when the analog output delay differs when the AD9161 is turned on and off
I think reading the values of addresses 0x037 and 0x038 and writing that value to 0x037 and 0x038…
Hi,
In my system fpga xilinx us+ and ad9164 the sysref is distributed by ad9508 such us the evb. I read the 0x37 and 0x38 registers and the value obtained are fc0, fe0 or f80 (after different power on). Are these values goods for subclass 1 sync or there…
For both AD9161 and AD9135 the number of bits per sample is 16 (NP=16). The core DAC truncates the number of bits to 11.