• AD9154-FMC-EBZ

    你好,购买了一套AD9154和ADS7-V2,参照https://wiki.analog.com/resources/eval/dpg/ad9154-ace-fmc-ebz 配置参数,ACE软件JESD PLL Locked 正常,但是DPGDownloder 中的sync status z状态始终为低,DAC0~3输出端口也无输出信号。请问是什么问题导致出错?期待你们的帮助。

  • register control word of DAC2/3 , AD9154 is not work.

    When ACE is used to set the register control word of AD9154,Under Link0, there are two pages, DAC0/1 and DAC2/3.When setting the data-format register, either directly or register debugI can only change the value of DCA0/1, which causes my DAC2/3 channel…

  • AD9154的SPI接口配置问题

    用Zynq7045的PS端的SPI外设配置AD9154读取芯片ID(0x005地址)返回值一直为FF,但是用相同的代码去读取AD9434就没有问题,能正常读取ID值,实在是搞不清楚问题会出在哪里

  • The register control word of DAC2/3 ,AD9154 is not work.

    When ACE is used to set the register control word of AD9154,Under Link0, there are two pages, DAC0/1 and DAC2/3.When setting the data-format register, either directly or register debugI can only change the value of DCA0/1, which causes my DAC2/3 channel…

  • The register control word of DAC2/3 ,AD9154 is not work.

    When ACE is used to set the register control word of AD9154,Under Link0, there are two pages, DAC0/1 and DAC2/3.When setting the data-format register, either directly or register debugI can only change the value of DCA0/1, which causes my DAC2/3 channel…

  • About AD9154 configuration.

    Hi,

        We have a project need to use a lot of AD9154, but this is the first time we use this chip, we purchased the ADS7-V2ER and AD9154-FMC BRD ,then we use the AD9154 SPI PRO software,it gave us a register configuration table, but according to the datasheet…

  • AD9154 DAC + PHY PRBS Testing

    I am using a AD9154 DAC and I am trying to use PHY PRBS Testing as described in the datasheet. The DAC PLL is locked but no valid PRBS sequence is fed to the DAC inputs.

    Every time when I finish the test by writing 0 to PHY_TEST_START the PHY_PRBS_TEST_STATUS…

  • Can AD9154 be connected to ADL5375?

    Hi,

    Recently I was reading the data sheet of DAC chip and modulator.

    There is a description in the modulator adl5375 as follows: "The ADL5375-05 is designed to interface with minimal components to members of the Analog Devices, Inc. TxDAC families. These…

  • ads7-v2er and ad9154-fmc brd quickstart.

    Hi,

          Our company has purchased ads7-v2er and ad9154-fmc brd. Currently, we are testing whether the AD9154 chip can meet our design requirements, but when using QuickStart, we encountered two problems.

    1: the output frequency is mixed with the input…