Yes, the AD9144 supports JESD204B Subclass 0 and Subclass 1 operations for deterministic latency. Subclass 1 provides synchronization to within ½ a DAC clock period and requires a SYSREF± signal to achieve this latency variation.
Yes, the AD9144 supports JESD204B Subclass 0 and Subclass 1 operations for deterministic latency. Subclass 1 provides synchronization to within ½ a DAC clock period and requires a SYSREF± signal to achieve this latency variation.
The AD9144 has 4 DACs and 8 available SERDES lanes with flexible interface configurations to meet various customer needs. The table below shows the transport layer JESD204B link parameters for each mode supported. These parameters are defined per link;…
Hello,
we are experiencing a problem similar to the one described in this post:
we have a custom board that uses the AD9144. We were able to…
Hi,
We are using AD9144 for prototype and I would like to know what is the purpose of this resistor R36 (25Ohm) at the center tap of the transformer and how the value is chosen.
Thanks in advances for your help,
XL
Hi team
I am looking to test AD9144 for PRBS7. For this, I am sending 32 bit PRBS7 data across 4 lanes (same data on 4 lanes) from the FPGA. On the AD9144 side, I am following Device Setup Guide section of AD9144 data sheet for details on setting up the…
Hi,
My requirements are:
- JESD204B operating mode 7 (LMFS=1241)
- DAC sample rate 250 MSPS
- Interpolation factor 8
- NCO 75 MHz
For now, I will configure the board without interpolation and NCO to make sure everything is set correctly.
Setup Environment…
Hi,
At our design we terminate AD9144 DAC outputs to 50ohm resistors to gnd, each. In our test we create CW square wave by toggling DAC output high and low at 237Mhz. We are measuring with spectrum analyzer on AD9144 50ohm outputs while all the rest of…
Assumed answered offline. Please re-submit if problems persist.
The AD9144 supports up to 1060MHz usable complex signal bandwidth. This allows customers to generate very wideband signals used in a variety of applications.