• RE: AD9125 as high-speed DAC with interpolator

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD9125 DAC Wake-up time after power down

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD9125 for generating Complex and Real IF with complex baseband inputs

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD9125 generate sine wave problem

    Hello,

    I'm using the AD9125 DA to generate a sin waveform.Use a 4x Interpolation,DACCLKP 400MHZ 、REFCLKP 100MHZ the DCI CLOCK 100MHZ,

    The  AD9125 SPI configuration is as follows:

    16'h0020
    16'h0000
    16'h0300
    16'h0CD1
    16'h0DD9
    16'h0AC0…

  • RE: Query regarding Sample Error Detection(SED) built in test in DAC AD9125

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Interface of Artix-7 FPGA (EK-A7-AC701-G) with DAC evaluation board (AD9125-M5375-EBZ) having FMC adapter board (AD-DAC-FMC-ADP ) to connect them

    Hi All,


    Is there any reference design available to interface Artix-7 evaluation board to DAC evaluation (AD9125-M5375-EBZ) board via FMC interface so that sinewave gerated from FPGA can be taken out from DAC.
    The DAC (AD9125-M5375-EBZ) Quick start guide…

  • AD9125 internal NCO

    Hello I have a development running inside a design house and I have been asked for this support:

    They are trying to use the internal NCO from the DAC to shift the frequency of the input sine wave.

    With that  it would be possible inject a sine to 7.8125Mhz…

  • AD9125 alias rejection using half band filters

    Hi,

    I'm using a common DAC clock of 370MHz, for IF generation of 70MHz and 205MHz.

    While generating the 205MHz, alias components are appearing at the output, which cannot be removed by and external discrete filter.

    I've attached a document to explain…

  • AD9125 Complex Mixer

    Hi,

    I'm using AD9125 to generate a complex signal at 70MHz.

    Is it possible to achieve image suppression @ the O/P if I'm feeding a complex IF signal to the DAC and use the complex mixer to generate the O/P?

    From the DUC I'll generate the complex…

  • AD9125 minimum DAC rate with internal PLL

    We're using an AD9125 DAC on one of our boards, with the DAC clock being sourced from the internal PLL, locked to an 80 MHz reference. We'd like to run the DAC in 2x interpolation mode at 160 MHz, but it looks like the internal dividers in the PLL can…