• RE: ad9125

    Hello,

    Assumed that his has been answered offline. Please let us know if this is not the case and we can open this back up.

  • RE: AD9125 latency

    Hi, by 1x mode,   bypass filters/modulator,   the latency will be 64 DAC clock cycle,  see datasheet page5. 

  • AD9125 输出 异常

    大家好,我调试AD9125的时候,输出为什么像是幅度调制了一个波形,具体如下文档所示,请各位大佬多多指教,多谢! DOCX

  • AD9125 输出异常

    大家好,我在调试AD9125的时候,输出频率是对的,但是波形像是幅度调制了,不知道问题在哪里,具体见文档,请各位大佬指教!多谢! DOCX

  • AD9125 internal VCO phase noise

    Hi,

    We are using AD9125 for our communication system transmitter.

    The upconversion to IF is also done using the complex mixer within the DAC.

    The reference clock to DAC ia 100MHz and we use the internal PLL to generate the internal DAC sampling clock…

  • RE: AD9125输出频谱异常

    This question has been closed by the EZ team and is assumed answered.
  • RE: AD9125 question

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD9125 Image Rejection

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Is AD9777 is better than AD9125 in ALL cases?

    I want correct reason which DAC is better Whether AD9777 or AD9125.