• AD9119 PLL LOST

    If we cold star with AD9119, PLL LOST will occur.
    Even if the initialization sequence was executed again, it remained PLL LOST.
    What kind of solution is there?

  • AD9119/AD9129 Availability

    Hello,

    When will be the AD9119/AD9129 and the associated eval board available ?

    Thanks

    Jur4ik

  • AD9119 output spectrum

    We use AD9119 output  32 channel J83 QAM signal, most time it"s good:

    but some times the 9119 output like this:

    Can anybody give us some ideas?

  • I250U in AD9119

    Hello,

    I'd like to ask you about I250U in AD9119.

    Q1.
    In Figure1 for datasheet, I250U connected 1.2V.
    What does it mean?

    Q2.
    Pls check Figure1 and Figure149.
    They have some differences around I250U, VREF and the comparator.
    Which is correct?

    Q3.
    Description…

  • AD9119 clocking with ADF4350

    Figure 148 in AD9119 datasheet shows a possible signal chain for the clock path base on ADF4350 PLL usage.

    Figure 22 in ADF4350 datasheet shows the PLL output stage.

    In my opinion, biasing is missing on the ADF4350 side since its output stage do not…

  • 关于AD9119评估板

    您好,我是一个在校学生,目前导师布置了一个任务,需要先对AD9119进行评估测试。我在贵公司的网站上没有找到AD9119评估板的原理图和仿真文件,请问我如何才能获得AD9119评估板的原理图?谢谢了!

  • Queries about AD9119/9129

    Hi, there

    We are planning to operate the DAC with the sampling rate of 2.7 GHz and in second nyquist using Mix mode.

     

     

    1) So we would like to know whether the part is capable of supporting instaneous bandwidth of 1 GHz (1.5 GHz to 2.5 GHz)

     

  • AD9119 IO spec missing

    I can't find DC specifications (Vih, Vil, Vol, Voh, leakage, and so on) for RESET and IRQ pins in the datasheet.

    In addition, there are two different indications about the pull-up value to use on IRQ pin (1k on p.9 and 10k on p.47).

    If a pull-up…

  • AD9119 and the Xillinx ML605

    I am interested in using the AD9119 with a Xilinx Virtex 7.

    I want  to generate waveforms using the Xilinx.

    I found the following set up on your WIKI site where the AD9129 works with a

    Xilinx ML605 board :

    http://wiki.analog.com/resources/fpga/xilinx…

  • AD9119/9129 and I/Q

    Hello Guys,

    I`m wondering if one can use the AD9119/9129 with I/Q (interleaving) input data?

    Thanks a lot!

    Juri