• AD9117: How do I estimate the overall DAC pipeline delay?

    How do I estimate the overall DAC pipeline delay?

     

    DAC pipeline latency is affected by the phase of the RETIMER-CLK that is
    selected. If latency is critical to the system and must be constant, the
    retimer should be forced to a particular phase…

  • RE: LTC5589 I/Q modulator with AD9767 TxDAC reference circuit design

    Hello  , 

    My apologies for the delay in response. In the shared article, you can disregard the Single-Ended to Diff Driver circuit & refer to the DAC reconstructed LPF and LTC5589 IQ modulator interface. I believe the DAC-TO-MODULATOR INTERFACING…

  • Can the AD9548 take 2.5V?


    Can the AD9548 take 2.5V on the output driver supply AVDD3 pins (31, 37, 38, 44) in CMOS mode? The datasheet specifically mentions 1.8V and 3.3V, but we're wondering if there is any issue with driving it at 2.5V to interface with AD9116 better and that…

  • AD9117 + interposer + ML605 + wiki issues = stuck

    Someone by email asked me:

    ------------

    I have the AD9117 Evalboard along with the FMC adaptor board and is using it in conjunction with the Xilinx ML605 board.

    Following the docs at:

    http://wiki.analog.com/resources/fpga/xilinx/interposer/ad911…

  • RE: Need high speed op-amp

    Dear Jay,

    thank you for your answer. There is no schematic but there is a block diagram like in attach file. Our aim is to change center frequency of the HMC899LP4 tunable filter.(Max. tunable supply +14V)  We think of use high speed DAC(like AD9116)…

  • AD9114/5/6/7 output stage voltage compliance

    I have a question regarding the main DAC output of the AD9114 / AD9115 / AD9116 / AD9117.

    Power is +3.3 V and for many reasons (cost, space, voltage supply and others) we need to get as much power as possible from the output stage to avoid an extra amplification…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • AD9717 and AD9117 CML Pins

    What is the purpose of the CMLI and CMLQ pins on the AD9717 and AD9117 DAC famlies and where do they need to be connected?

  • DAC Calibration

    Some high speed DAC have options for auto-calibration. Why and when should I use this option?