• AD9106

    I encountered some problems when using registers to generate sine waves. At first, when I set 0x3E to 0021, and 0x3F to 0000, a 50k sine wave appeared. I want to change the DDS_ TW32 and DDS_ The TW1 value can get the frequency I want, but I can't get…

  • AD9106 Evaluation Board CD lost

    Hi all:

     I bought the AD9106-EBZ Evaluation Board , but there is no AD9106 Evaluation Board CD in the box, where can I download the material of AD9106-EBZ? THANKS

  • clock setting of AD9106

    Hello,

    I want to get a sawtooth at 10Hz and I use the clock of 100M Hz. By configuring registers of 0x28 and 0x29 I required the minimum frequency is approximately 100Hz. Excepting changing the clock source, is it possible to reduce the frequency to 10Hz…

  • DDS Phase offset registers AD9106

    AD9106 datasheet indicates registers from 0x40 to 0x043 allow phase control for each DDS output available, but when changing values on those registers phase is not changing at all (I compared with other output withput phase offset). I'm able to configure…

  • AD9106 Offset Phase registers

    Hi

    AD9601 datasheet indicates registers from 0x40 to 0x043 allows phase control for each DDS output available, but when changing values of those registers at configuration procedure, it does not control phases at all. I did a reading from mentioned registers…

  • clock of ad9106

     how to adjust the frequency of sawtooth wave if i want to use sawtooth wave generator.

    and If I use the sram to store sawtooth waveform data, how do I configure the sawtooth frequency?

  • Using DDS of AD9106 to generate waveform

    Hello everybody,

    I tried to communicate from FPGA to AD9106 via SPI and after transmission of values (which are in the example6.regval). I do write Sequence in the order of SPI configuration and the simulation waveform is correct. But I can not have any…

  • AD9106 SRAM waveform output not working

    I want to generate a continuous waveform from the AD9106 that outputs the waveform loaded into the device SRAM.
    I configure the WAVE SELECT register, 0x27, to run a waveform read from RAM between START_ADDR1 and STOP_ADDR1 for WAVE_SEL1.
    I load the 12…

  • Why the AD9106 current output is not 12 bits

    HI

    Why the AD9106 current output is not 12 bits,The result is 10 bits.

    I change the gain of output current by writing register 0x0035

    WriteToAD9106(0x0035,N*4); //DAC1_DGAIN
    WriteToAD9106(0x001d,0x0001);

    I measure the voltage at both ends of the external…