• AD9082 Maximum IBW

    Dear Team ,

    Could you please clarify below mentioned doubts.

    (1) Why 4GSPS only on VCU 118 ? Is it not possible to give maximum 6 GSPS as the JESD is already type C.

    If this board not supporting then which Xilnix board supports this maximum 6 GSPS ADC…

  • AD9082 TX/RX 8Ghz

    DEARS.

    What does "Useable analog bandwidth to 8 GHz" mean as stated in the datasheet?
    Can I use the AD9082's TX/RX frequencies up to 8Ghz?

    Thank you.

  • AD9082 JESD204C FEC support

    Hello.

    Does the AD9082 support JESD204C FEC?

    Also, does Analog have any data on the expected BER rate of the SERDES links, for example a measurement from the EVM?

    Thanks.

  • AD9081/AD9082 Evaluation Board Schematics

    Where can I find the schematics/BOM/Gerbers etc... for the AD9801 & AD9802 Evaluation Boards ?

    I did see the related post and answer:

    Design Files: https://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL…

  • AD9082-FMCA-EBZ with ADS9 evaluation board: MatLab API

    Hi,

    I have recently configured the boards:  AD9082-FMCA-EBZ with ADS9 evaluation board using MatLab as provided by a user guide. I have two questions thou:

    1) If i am configuring the boards using MatLab API, why do i need to upload the FPGA image? What is…

  • pyadi-iio/libiio program AD9081/Ad9082

    Hi:

       I am trying to configure and program an AD9082 DAC on ZCU102.  I am familiar with AD9371/AD9361-iiostream.

    But I have not seen any reference libiio code for programming the AD9081/AD9082 with libiio.  I have found the pyadi-iio 

    software for these AD908x…

  • Is there data for the IIO-DAC latency for AD9082?

    Can I find information describing the latency using pyadi-iio or libiio to stream output to the AD9082 DAC?

    Is there a way to configure IIO-Oscilloscope to provide the information?

    Thanks,

    TW

  • Question about exact part number of AD9082 on AD9082-FMCA-EBZ

    Hello,

    My customer will purchase the AD9082-FMCA-EBZ , but before then, they want to know the exact PN of AD9082 device.

    As you know, there are 4 types of AD9082 devices are existed like below.

            1. A D9082BBPZ-4D2AC : Tray , 4D2A

            2.  AD9082BBPZRL…

  • AD9082 washing/cleaning

    Hello.

    After population, can the AD9082 be washed to remove flux residue? 

    Can an aqueous wash be used, with a saponifier?

    Can a solvent wash be used?

    Thanks.

  • AD9082 JESD204C link fails when changing decimation ratio at runtime

    Hi.

    I am using the AD9082 in dual link mode. I would like to change the decimation ratio of the FDDC on the fly, without changing the JESD204C data rate. The AD9082 supports this for power of two decimation ratios, as it can repeat samples using the upsampler…