• AD9081-FMCA-EBZ Fan Connector

    Hello,

    The fan cable that came with with the board comes with two wires - Red and Black.  When I insert the fan connector into the board and perform a continuity measurement from the Red wire side to GND I get continuity.  So either the wires were put into…

  • AD9081 TX and RX Sample Rate - Low sample rate

    I want to change the TX and RX sample rate of the AD9081 over the Zynq-7000 SoC ZC706 channels.

    Following the explenation in this post (here), I triyed to change the interpolation and decimation figures in the devicetree (for main-data-paths and channelizer…

  • AD9081-FMCA-EBZ VADJ

    I'm using the AD9081-FMCA-EBZ with a Xilinx ZCU216 where i'm having to use a HiTechGlobal FMC extender/splitter so that the AD9081 board doesn't foul the QSFP cage on the ZCU216. It looks as if the ZCU216 can't determine what the VADJ voltage should be…

  • JESD204C DAC transport layer for ad9082/ad9081.

    I'm interfacing the ad9082 eval board with the zcu102 carrier. I am developing firmware using the Xilinx JESD204C cores. I have integrated the RX JESD204C core in ZCU120 and used a transport layer generated by JESD204 Transport Layer Generator v1.…

  • RE: AD9081 no-OS ADC sample capture

    Hi  

    Good news!:

    I created a 50MHz tone within the FPGA, sent it out the RFSoC DAC, connected the DAC output to one of the ADC inputs on the AD9081 eval board and sure enough, I can see those samples at the output of the ADC transport layer component…

  • AD9081/2 ADC Valid Dual Link Modes?

    I'm interested in running the AD9081/2 ADCs in dual link mode. However, the user guide doesn't call out which JESD modes are valid for dual link or not. Which ADC JESD modes are valid for dual link?

  • Which folder should be used to as import for Vitis for ad9081

    Hi everyone,

    I have come from using SDK and now using Vitis, but I cannot find any guidelines as to how to port the no-os project after is made from the Makefile. Like which folder should I port as they are many generated folders in the build directory…

  • Programming AD9081 filter via ACE GUI

    Hi, I originally posted this the high speed converter forum but did not get a response so am reposting here:

    Hi,

    Could I have a bit more info on how to configure the programmable filter for the AD9081 via the ACE software/plugin (using AD9081 eval board…

  • Programming AD9081 filter via ACE GUI

    Hi,

    Could I have a bit more info on how to configure the programmable filter for the AD9081 via the ACE software/plugin (using AD9081 eval board + ADS9 setup).

    I can successfully load a 192-tap filter and receiver one channel as described in the wiki…

  • RE: Reference design for AD9081 EVB with EEPROM

    Hi, the EEPROM has board information that tells our evaluation software (ACE) what board it is interfacing with so it can open the correct plugin. it isnt needed if your end system implementation doesnt conform to vita57.x spec. if you intend to use the…