• AD9057: Aperture uncertainty

    1) Do you have any additional information of the influence of the temperature
    over the "Appertur Uncertainty Jitter)?
    2) When you apply an input votage of 3V, what is the "shortest" time needed to
    "Track-and-Hold" the input signal…

  • AD9057: BIAS out grounding and drive current

    In a prototype construction we are using an AD9057 A/D converter and my
    question is can the BIAS OUT (pin 6) be grounded ? Or will this degrade the
    performance of the A/D converter (vref out/in)?

    I also would like to know if the internal reference…

  • AD9057 noise

    Hello,

    I am trying to use an AD9057 analog-to-digital converter (-80 grade) with an Encode Clock of 80MHz, 3.3V square wave.

    I get a terrible clock return on the input signal itself. If I monitor the input signal, for example a 1Vpp sin waveform at…

  • What is the maximum operating supply volatge (Operating supply voltage range) for AD9057?. The datasheet only specifies the absolute maximum ratings.

    The datasheet only specifies 5V as analog power supply and digital power supply as 3V to 5V. #AD9057 #highsspeed adc

  • AD9048 - any pin to pin replacement

    Hi,

    I saw on AD9048 product page that this chip is obsolete. ADI suggested to use AD9057, but it is not for pin to pin. I would like to verify from ADI side that if there is really no pin-to-pin replacement for AD9048?

    Thanks!

  • (AD8206/AD8211)Why did you change the datasheet?

    Hi !

    I have some questions about ADI datasheet.

    Our team are checking the datasheet because if the datasheet was changed we have to explain the changes.

    And today , we found many datasheet was changed.

    For just one example , AD8206 datasheet was changed…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…