FAQ
Hello!
As per datasheet:
AD9042: 41MSPS, 595mW
AD9254: 150MSPS, 430mW
If I use these ADCs at a lower sampling rate say 20MSPS (if its possible) will the ADC run at a reduced power? If so, what will be the power consumption in the case of reduced sampling…
Hello AD Experts,
I am using AD9042 for Digital Control of Power Supply.
I am using FPGA as a digital controller which operates on 3.3V only. But here it is mentioned that the AD9042 requires 5V analog and digital power supply.
But absolute maximum…
不建议直接连接使用。建议使用电平转换芯片进行处理,如ADI的ADG3300系列,或者其他厂家,如TI的SN74L系列电平转换器件。对于AD9042其实也可以考虑使用串联电阻的方式进行处理,但是要考虑因为电阻和分布电容带来的滤波效应,以免影响数字信号的正常传输。
Hello,
I required an high speed ADC with bipolar analog input ranging from -V to +V. I was considering AD9042 but later on it came to my notice that it does not take in bipolar analog input. So, right now I am considering the following ADC's for the…
Hello,
I’d like to use my C code with pluto to build a ‘’simple’’ stand alone receiver.
I read a lot of Q&A and your answer here: https://ez.analog.com/university-program/f/q-a/104394/how-to-implement-c-code-examples…