• AD8619,AD8694 Noise immunity at portable radio frequency band

    Hello.

    The customer requested as follows for AD8619 and AD8694..
    Do you have these data?
    Please see to “Background” for detail information.

    Q1: Why AD8619 and AD8694 has tolerance for noise at high frequency band(144MHz~3.6GHz)?
    Q2: The noise immunity…

  • RE: CN0510/AD5941 Loss of accuracy after amplifying disturbance current

    Hi,

    Yes, your analysis is correct. Increasing the current through the battery is increasing the differential voltage across the cell and also across RCAL. The gain stage implemented by the AD8694 is increasing the current beyond the limits of the AD5941…

  • RE: ad823an 4OPAMP single package

    Some suggestions:

    AD8608

    AD8694

    AD8630

    AD8604

    I'm assuming you meant TSSOP14

  • RE: ADMP441, SSM2529 Speech transmission

    Thank you for a thorough explanation.

    I have looked further at your catalog of op-amps. Since I am designing a portable unit, I examined the following, with 5 V supply:

    AD8605/AD8606/AD8608, AD8691/AD8692/AD8694, AD8655/AD8656, and the ADA4075-2.

  • RE: ADA4530-1 Die level option

    Hi Mika,

    We currently don't have ADA4530-1 in a die level and I'm  not sure if we will have in the near near future. However, i found these few devices with 1pA typical bias current operational amplifiers in die/chipscale package. We have AD8691…

  • RE: CN0276 EXC filter design

    Hi firman,

    Figure 12 is the phase shift between the AD2S1210 EXC and SIN pins which shows how the noise from EXC pins of AD2S1210 was improved.  This is because of the amplifiers which acts as an active filter found at the resolver excitation(which uses…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…