对着CN0343电路图做仿真的时候发现好多元件找不到请问该到哪找?
I have an amplifier AD8692 used for voltage sensing with opto coupler for isolation. it is quite unstable in the whole range of input voltage.
i have tried to simulate it in ltspice and its quite stable. maybe the model is not so perfectly represented…
Hello,
For now, there is no equivalent amplifiers of AD8692 and AD8397 (from CN-0276) with extended temperature range. But, here is the list of the rail-to-rail operational amplifier with extended temperature range which can operate from -55 °C. The closest…
I can't find them for AD8692 opamp and ADCMP608 comparator. No special footprints, I just wanted to double-check.
Hi firman,
Figure 12 is the phase shift between the AD2S1210 EXC and SIN pins which shows how the noise from EXC pins of AD2S1210 was improved. This is because of the amplifiers which acts as an active filter found at the resolver excitation(which uses…
买了一批AD8692ARMZ,MSOP-8封装的,批量焊接时,发现8个引脚的端面不上锡。经过仔细观察发现端面呈现黄色或黑色,咨询一下行内专家说是芯片引脚镀了镀层后切割的。
现在质量要求芯片引脚的端面需要上锡50%以上,请ADI专家给出解决办法?
Hi Mika,
We currently don't have ADA4530-1 in a die level and I'm not sure if we will have in the near near future. However, i found these few devices with 1pA typical bias current operational amplifiers in die/chipscale package. We have AD8691…
公司一个项目用到AD2S1210,目前正在熟悉阶段。今天使用CN0276推荐的电路进行试验时,发现读到的角度总是比实际给的角度始终大180°(如实际位置为10°,用AD2S1210测的是190°,实际位置为45°,用AD2S1210读到的位置是225°)。我对CN0276中给的电路仅修改了激励放大系数(图1)和相应的sin和cos系数(图2,旋变压比为0.5,到sin和cos引脚的VP-P为3.1V),使用2.5kHz的激励,锁相在±44°内。…
首先说我的方案,是参考AD2S1210给的方案,基本照搬过来的,输出运放使用的AD8397,输入运放使用的AD8692。
问题现象是AD2S1210在静止不动时,测量跳变非常小,只有1个Bit;当我开启电机时,会发现有某些位置出现大的跳变,导致测量位置不准确。我用示波器看了激励波形和正余弦的波形,用差分探头看的,质量很好,但是转的时候由于不好确定时间,没能抓到位置跳变时候的正余弦波形,只能大概看一下,波形是好的。
问题1:可以看到旋变的位置跳变是有一定规律的,但又不是电机的一圈,已经转了多圈…
ADI放大器给我的印象就是产品丰富,可靠性高。
再说说如何选择不同的放大器。
(1)确定放大器的用途和应用场合:放大、滤波、积分、隔离,还是低频、高频、音频等。
(2)确定放大器的输入输出、电源、使用温度环境范围。电源分单电源和双电源。
(3)确定关键技术指标。比如滤波电路需要首先考虑放大器带宽,电荷放大电路首先考虑低失调电流等。
(4)根据PCB和产品尺寸,确定封装形式。
(5)结合产品手册选型。
实例:在设计一个传感器的调理电路时,需要用到放大器进行放大,信号频率不高<1MHz…