AD8691不错的选择,收藏了
AD8692用AD8691的spice模型,AD8692是双运放,AD8691是单运放。
其他器件如果在LTspice中找不到,可以到ADI官网上下载相关spice模型(.cir文件),每一个运放的页面基本都能找到相关的spice模型(一般在Datasheet下面)。然后将cir文件导入到LTspice中自建电路模型。
附件中是如何在LTspice中导入模型文件的方法:PDF
Thank you for a thorough explanation.
I have looked further at your catalog of op-amps. Since I am designing a portable unit, I examined the following, with 5 V supply:
AD8605/AD8606/AD8608, AD8691/AD8692/AD8694, AD8655/AD8656, and the ADA4075-2.
…Hi hulala,
Because the AD8691 is a CMOS amplifier, it should have very high input impedance. I do not think there will be any problems with interfacing this to the ADMP411. I have communicated with the engineer of this part to try and see whether I…
Hi there,
I have a quesion about AD8691.
http://www.analog.com/static/imported-files/data_sheets/AD8691_8692_8694.pdf
Looking at the input voltage range of the datasheet, it says +3.9V(Max) at Vs=5V.
And also this is specifired at T A = 25°C.
I need…
Hi Mika,
We currently don't have ADA4530-1 in a die level and I'm not sure if we will have in the near near future. However, i found these few devices with 1pA typical bias current operational amplifiers in die/chipscale package. We have AD8691…
The first thing to compare is the Signal-to-Noise and Distortion (known as SINAD) of the ADC to the distortion and noise (THD+Noise) of the op amp. You want the SNR+THD of the amplifier to be less than (i.e., more dB)that of the ADC. For example, the…
AD7998 datasheet says that the voltage range for external reference can be any between 1.2 and VDD. I acquired an eval-ad7998 board and rewired one of the digital potentiometer to work as the external reference voltage at 1.0 vcc (my magic number). The…
I am a digital designer, and a bit out of my element using op amps.
I need to amplify a pulse stream using a single op amp stage [board already designed/fabbed around an SOT23-5 package]. I am currently using
I need the highest gain I can get [10-20mv…