• AD8682 input range for Vs=+/-13V

    1.
    Please write your questions or comments here: The datasheet of the AD8682
    stipulate that with a power supply of +/-15V, yhe maximum negative input
    voltage is -11V. What would the limit be with a power supply of +/-13V? What
    happen…
  • RE: 这11大应用领域,你在里面么?

    关注领域:关注仪器仪表和测量

        因为本身从事的就是仪器测量检测方面的工作,对该方面的关注自然就高。在工作中,经常用到ADC、OPA等各类器件,一直相信ADI出色的模拟信号处理能力,芯片运行稳定。不管是仪运放AD620、低功耗运放AD8682,还是其他ADC,AD7766等等。

        目前正在用AD7766这款ADC,24位,8.5mW,低功耗。

        一直都喜欢ADI!

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • ADI运算放大器选型指南

    ADI运算放大器选型指南

  • Is ADP2291 working as expected in the datasheet or its examples are fail?

    Hello Everyone,

    Im working on a battery charger circuit. I set completely the figure-22 and the figure-23 in the datasheet. So more than hundred try and later than weeks. The circuits are not working as expected. This part is important "The circuits are…

  • Noise optimizing AD8599 &&

    Good day,

    I have a task to optimize noise in BW 10Hz - 10kHz.

    Voltage gain shall be around 20..50. OA connected directly to source of signal,

    which has impedance 1kOm DC and 50Om AC. OA connected to middle point of R1/R2 divider,

    where R1 connected…

  • ADI芯片辨识、型号查找

    看看截图: