Hello,
I have some questions about the AD8675 (or 8676) and its popcorn noise.
I plan to use an AD8676 (or AD8675) in order to measure [0,1Hz;10Hz] noise of a low noise voltage source. I have chosen this amplifier as, according to the datasheet, it has…
Hi, I am designing a high current driver after a precision DAC (AD5781). I found the circuit from AN18: Power Gain Stages for Monolithic Amplifiers. In Figure 02, It uses a current boost design of NPN + PNP after a high current buffer LT1010, which is…
I found that in CN0200 and CN0191, AD8676B and AD8675 are used for both force and sense pins and the output buffer of AD5781/AD5791. The specification of AD8676 is superior, though, the slew rate is limited. We are considering replacing the amplifier…
请问用一路ADR4550B(Isc=10mA)分别产生+5V和-5V的基准电压,该两个基准电压后接AD8675的单位增益放大器。产生的VREFPS、VREFPF、VREFNS、VREFNF能否作为16路DAC AD5791的共同基准输入端。 LTSpice无ADR4550的模型,用ADR4525代替仿真。
2. Is the front-end amp in a de-compensate state? i.e., the minimal gain of front-end amp should be at least 5 or more. Do I need a small capacitor between Vout of ADA4637 and the inverting pin?
3. I would like to use AD8675 as the front-end op-amp, where…
Hello to everyone,
I am using the AD8675 operational for a project simulating on Tina software.
I noticed that the measured input voltage offset (115uV) is different to that indicated on the datasheet (Typ=10uV, Max=75uV). The simulation temperature is…
Hi,
Can you check/probe on the DAC output itself if it is able to reach reach 5V, it should be. I think that the problem is with the setup of the buffer amplifier. If you'll look at the ds of AD8675, the input voltage range spec is 3V max for +/-5V input…