• RE: Will there be a dual version ADA4627-1.

    FormerMember
    FormerMember

    Bryan,

    I wish you would have gotten a name so I could track this down further.  Was it a local field office

    or an office in Norwood?   Which department?  That is certainly unacceptable behavior.

    I was the product line apps engineer for the ADA4627-1. 

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • 10/12/16 Challenges for Electronic Circuits in Space Applications

    This webcast provides insight into the challenges engineers encounter in implementing circuits for space applications. Concerns about reliability, radiation effects and the ability to tolerate harsh environmental conditions requires special attention…

  • Is ADP2291 working as expected in the datasheet or its examples are fail?

    Hello Everyone,

    Im working on a battery charger circuit. I set completely the figure-22 and the figure-23 in the datasheet. So more than hundred try and later than weeks. The circuits are not working as expected. This part is important "The circuits are…

  • ADI运算放大器选型指南

    ADI运算放大器选型指南

  • Noise optimizing AD8599 &&

    Good day,

    I have a task to optimize noise in BW 10Hz - 10kHz.

    Voltage gain shall be around 20..50. OA connected directly to source of signal,

    which has impedance 1kOm DC and 50Om AC. OA connected to middle point of R1/R2 divider,

    where R1 connected…

  • ADI芯片辨识、型号查找

    看看截图: