• AD8666 LTSpice transient analysis failure

    I'm trying to simulate a simple unity gain inverting amplifier using the AD8666 with +/-5V power supply.  Feeding a 1 V amplitude sine wave centered at 0V generates an output waveform that seems to have problems on the negative side.  Increasing the…

  • AD8666: Supply range

    Can the AD8666 work at supply voltage below 5V (single supply), in particular
    down to 3V.

     

    No AD8666 is not suitable for 3V supply, the supply range is from 5V to 16V.
  • AD8666 LTSpice Model

    Is there one available (I don't see it in the LTSpice library)? If not, do you recommend another similar part to use for simulations?

  • AD8666轨到轨运放饱和电压误差大

    我用的是AD8666轨到轨芯片,电源供电10.6V,该电源是由MC33063出来的电压供电的。当调整Vin的输入时,Vout最大只能到9.2V,与电源电压差了1.4V,我看文档里面写的运放输出最大值与电源电压就差几十mV,为何会偏差这么大?

  • Comment on AD8666: Supply range

    But  I am using AD8666 @ +3.3V single supply in my application.. how is it possible then? 

  • RE: Problems on my ad5933

    No need to worry about R3 and R4, those can be of any value as long as they are not too low to drain too much current from power supply and not too high to generate noticeable voltage drop passing bias current from the OPAMP non-inverting input (<1pA…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • ADI运算放大器选型指南

    ADI运算放大器选型指南