Q
Our customer wants to use AD8662 with +/-5V supply voltage.Datasheet mentions 16V supply voltage range.
Can you confirm that it is OK to supply +/-5V for this device ?
Are there some cases with AD amplifiers where it is not possible…
当我环顾四周,却始终无法找到我的梦想之车时,我决心亲手打造一辆—费利.保时捷
摘要 :本文通过对PCM-D50进行电路改造,使之具有和更高级机种PCM-D1相同的回放电路。在牺牲部分续航能力的前提下,使D50在现有的电路上更充分地发挥硬件潜能,达到音质改善与驱动能力提高的目的;关于改造的理论依据和改造后的性能分析评价也将在本文内详述。
提纲:
一,升级理论
tpsamuel,
If your resolver requires 4.25VRMS (differential) then that is about 6Vp (12Vpp). The RDC swings between 7.2Vpp to 8.0Vpp differentially, natively which means you would need about 1.5x gain so the 15.4K option should be sufficient for your needs…
EXC和后级AD8662电路可以先不挂旋转变压器,挂普通的电阻负载测试下,看看基本电路能不能正常工作,如果没有问题,再挂旋转变压器,从你的测试看,可能基本的电路有问题
1.首先建议将AD8662的共模输出调整成6V,这样保证在12V供电时输出摆幅最大。
2. 根据8V励磁电压以及负载电阻来计算,目前选择的三极管的驱动能力可能是不够的。建议更换成更大电流能力的三极管。
您好,谢谢回复!
功放之后接的就是旋变没有其他负载。驱动能力不足应当是硬件问题了。我参考电路笔记CN-0192设计的一级放大电路(如前面评论的图所示),现在打算把一级放大改成二级放大,即用两个AD8662来进行放大,请问这样是否可行?