本电路图是功率稳定完整描述图,图中绿色标注部分为接口的相关说明,基本原理就是通过光电二极管采集的电压同设定光强电压做对比,最终将输出电压输送给光栅,以此来调节激光器的光强。
然而涉及到芯片的一些接法实在不知道原理是什么,因为是从其他控制器直接copy过来的板子,所以不知道有些接法不知道是对是错。
请教大神描述一下一些接法原理:ad8610的接法网络,tl084, ad823,还有ad712的接法,这些都是为了做什么呢?
电路图附件表示中。其中ad8610部分在最下方。
I use AD8620 as a cross-coupled single end to differential coverter as following figure, but it doesn't work. what should I pay attention to? can I use other general OP (such as LF353D) to replace the AD8620? I need +/-12V power supply and both of them…
说实话,AD8620是唯一的低功耗(Iq=3.5mA),高压摆率(SR>50),高带宽,低噪声,高容性负载驱动力各个指标层面上最优的产品了。。。但是就是价格比较感人,我们的设备原先使用的AD8066,后来换了ADA4610-2发现压摆率可能上不去,很有可能要吐血上AD8620了,一个板子8片。
真心不错的产品。要是ADA4610的压摆率能到35(仅仅增加10,为了与AD8421匹配),我们就能用了,哎,差一点心疼死人啊
最近玩音频运放,看到网友分享的AD8620试听评价,很发烧很专业! ADI的专家怎么看?大家怎么看?
http://www.erji.net/thread.php?fid=6
迎来了两只AD8620的运放,几经辛苦焊上镀金脚座后,便迫不及待地插上cd机,现在谈一谈这对ic的听感:
开声用一张关正杰的黑胶系列《名曲选第二辑》的曲目15《渔舟唱晚》,一开场的海浪声后~接住的一段古筝,只“见”声音清澈,通透感十足,而且声像阔而深;人声部分展现出十分清晰而沧桑的线条感,而且声像大而不冲,感觉醇厚…
Hi Jonathan,
The AD8512 and the AD8620 are not pin-to-pin compatible with LTC2055 so I would not like to use them.
I'll try to test with AD823A.
Regards,
Kazu