Hello,
Is it OK to apply 5.5V power supply to AD8617?
It is not clear in datasheet whether maximum power supply should be 5.0V or 5.5V.
Best Regards,
Hello,
Is it OK to apply 5.5V power supply to AD8617?
It is not clear in datasheet whether maximum power supply should be 5.0V or 5.5V.
Best Regards,
I'm surprised it is doing anything.
-- You need at least 5V across the part to wake it up
-- It is not RR input; you need to stay at least 1.5V away from either rail.
Try an ADA4084-2 or an ADA4528-2
For the LMC662,, you could also look at:
ADA4691…
In AD8629 Spice model the Flicker noise parameters and Noise models such as the ones mentioned in AD8617 SPICE model has not been given in AD8629 Spice model. Hence i here by request you to kindly provide the AD8629 SPICE model with all the noise parameters…
Hi,
That was a very helpful piece of information.Thanks.
Elias,
What does TRRS mean??
What is your highest signal frequency?
Depending on whether you need to go to DC or not and can AC couple, you could use op amps
that have millivolts of offset, rather than <100 uV which drives up the price.
Also…
Hi Ching.
First of all, the initial requeriments of my project:
- 8 universal analog inputs (RTD, TC, 4-20, Voltage). 3 header pins.
- Each channel can be configurated independently for RTD, TC ... measurement mode. Another choice if this option…
AD600 |
AD602 |
AD603 |
AD604 |
AD605 |
AD8264 |
AD8330 |
AD8331 |
AD8332 |
AD8334 |
AD8335 |
AD8336 |
AD8337 |
AD8338 |
ADL5246 |
ADL5330 |
ADL5331 |
LTC6412 |
HMC6187G |
HMC997G |
HMC996 |
HMC694G |
AD8368 |
AD8351 |
AD8367 |
AD75071 |
AD552… |
你知道心源性猝死(SCD)吗?
心源性猝死是指急性症状发作后1小时内发生的以意识突然丧失为特征的由心脏原因引起的自然死亡,而且心源性猝死90%以上发生在医院外,但是这类猝死病人的黄金急救时间只有5-10分钟,超过10分钟的抢救存活率不到1%。
当发生心源性猝死(SCD)时,唯一的救治手段是胸外按压+心脏除颤,及时除颤是迄今公认制止心脏猝死的最有效方法。
对此,ADI推出了自动体外除颤器(AED)解决方案,可以自动诊断可能危及患者生命的心室纤维性颤动和心室性心博过速两种心律失常症状。
自动一词提示器件可以自主分析患者状况…