I have searched the internet for hours upon hours to find answers to my questions with no luck... Below are 2 circuits that are a part of a project I am working on.... These are the interface circuits between my system and a balanced signal TDM box with…
Hi,
How can flicker noise be calculated on AD8608 for low frequency applications?
https://www.analog.com/media/en/technical-documentation/data-sheets/AD8605_8606_8608.pdf
among the features I found this:
The Peak-to-Peak Noise voice for frequencies…
想使用AD8605 ad8608 进行光电光电二极管前置放大器的设计 它的外围电路该如何设计 比如 Cf Rf 还有输出端滤波等等 有没有相关的参考设计和说明文档 谢谢
Some suggestions:
AD8608
AD8694
AD8630
AD8604
I'm assuming you meant TSSOP14
Hi Jerad,
Why do we have AD8608 opamp on ADAU1446 evaluation board? Can these act as preamp for microphone?
Thanks
The CN0350 use 4 AD8608, so the Power dissipation=4*3.3V*1.2mA=15.84mW.
Am right?
And does any tool can calculate the Power dissipation of the entire system?
Lin
Your computation for C2 and the system error is correct. The system error arises from multiple sources such as temperature drift of the resistors and voltage reference; and offset drifts from the AD8608.
Regards,
Nikko
ok thank you so much! last thing If I had to use a quad-opamp AD8608 to perform the translation of the level from 5V to 3.3V how to estimate the flicker noise since the application is at low frequency? the datasheet tells me to consider it.
按照AD7689-CN0254文档做了一个PCB样板,焊完板后在调试中发现前端不正常,开始认为是前端IC(AD8608)有问题,换了也不正常,