• 我选用了一款AD8607的芯片,想仿真,用什么软件呢

    TI公司有一款仿真软件叫TINA,可以很方便的仿真TI公司的芯片。那么请问ADI公司是否也有这样的仿真工具呢,我想仿真AD8607

  • 最爱ADI放大器-AD8607

    单就运放而言,在这几家最大的模拟厂家里,ADI的运放种类是最全的,每次总是能选到最合适的。

    我做的直流精密测量方面的比较多,我选用AD8607这款。近几年,在做水质分析仪器,只要是直流放大的应用,都上AD8607毫不犹豫,每个项目都很好的满足要求。

    我大概总结了一下,AD8607有这么十大优点:

    1. 低失调,低温漂

    2. 单位增益稳定(可用于跟随器)

    3. 输入输出都能轨对轨,R-R Input,R-R Output

    4. 功耗低,但输出驱动能力还强

    5. 低压,单电源(现在这可能不算优势了…

  • Simultaneous measurement of pH and ORP

    Hello, I use CN0326 to measure pH (mV), the result is very good, but I want to measure and add ORP parameters on the same circuit at the same time. i changed Opamp AD8606 (1 channel) to AD8607 (2 channel). Then connect two pH and ORP sensors simultaneously…

  • AD8307: What is the input impedance of AD8307?

    What is the input impedance of AD8307?

     

    We don't specify the input impedence directly, but as it is an input to an
    operational Amplifier, its in the Mohm range. More significant is the input
    bias current which for the AD8607 ( for…
  • RE: Using The ADA4177-2 as a buffer, outputs don't exactly follow inputs

    I'm surprised it is doing anything. 

    --  You need at least 5V across the part to wake it up

    --  It is not RR input;  you need to stay at least 1.5V away from either rail.

    Try an ADA4084-2 or an ADA4528-2

    For the LMC662,, you could also look at:

    ADA4691…

  • RE: 分享您最中意的ADI资料,赢跨年好礼

    已经做过好几个项目了,感谢AD8607,非常出色的应用在直流放大方面。优点有:功耗低,但输出驱动能力强;共模电压输入范围无限制;很高的共模抑制比,电源抑制比;极低的输入偏置电流Ib。
  • AD8232's IAOUT has some random noise

    I bought AD8232 EVAL and checked ECG signal under the following configuration.

    <Configuration>

    3 electrode connection

    DC leads off detection

    FR disable

    During measuring ECG signal on IAOUT and OP AMP OUT, there are random noise on both signals…

  • RE: AD8541 AD8542 AD8544 noise (low frequency)

    I was thinking about AD8539, but AD8607 also looks good. I will take this op-amp for RLD circuit.

    Thank you Harry!

  • AC analysis of transimpedance amplifier LT-SPICE

    Hi 

    I am working on a design that requires integrating transimpedance amplifier. I have already designed the board but I am having serious issues with the oscillations. 

    I would like to simulate my circuit in LT-SPICE & observe the effects of various capacitance…

  • Analog switch to detach EEG electrodes from circuit

    I have what I think is a fairly unusual problem. I have a 2 channel EEG with a right leg drive. I am using AD8226 and AD8607 for the design. At some particular point in time, I need to do the following things with this machine:

    - transform the EEG electrodes…