问题一:经查阅资料,反馈回路并联电容电阻起低通滤波器和相位补偿作用,计算得到低通滤波截止频率位6kHz,但经实验证明,200kHz信号正常进行放大,这个电容的准确作用是什么?该如何判断?
问题二:反相输入端仅提供100Ω电阻,LTspice软件仿真结果如下图所示,信号因放大倍数过大发生失真,但实验验证200kHz信号可以正常进行放大,该放大器是如何进行工作的?
如图所示,在输出与反相输入端的反馈回路之间有一个电容并联于电阻上,查阅资料有的说是低通滤波作用,截止频率是6kHz左右,但是200kHz顺利进行放大,也不满足积分电路的大小和时间常数,这个电容是起什么作用?该如何判断?
第二个问题:在反相输入端输入电阻是100欧姆,仿真时信号放大倍数太大失真,但搭建最小系统板却显示200kHz信号正常放大,该放大器是如何进行工作的?
I have some questions about AD8606 output current.
There is a spec " output current".
What's the definition of this ouput current?What would happen if it's exceeded?
And one more thing,
the output current is ±80mA at 5V supply and…
In the above circuit the underlined IC AD8606 is getting heated up. At the node marked (low pass filter output) the current is high when i checked in ADIsimPE simulation software. how can this problem be overcomed?
原理图如左图所示,需要实现一个小电流输入端的电压跟随器
Rload在100kΩ左右,电流在100nA~10uA的范围;电路目的为在已知输入电流的情况下,测试负载的阻抗。
第一次使用AD8606构建,结果如下,使用吉时利DAQ6510测试
图中红色线条为理想情况,黑色线条为AD8606构成的跟随器测试情况。
曲线不合推测为AD8606最低电压输出相对较高所致,如下:
最低输出电压为40mV,与曲线最低电压基本一致。
现在尝试用LTC6268来构建,但是并未在数据手册上找到相应的最低输出电压的参数…
It is probably worth trying. Pmodia uses the AD8606, which might not be the best OPAMP for this type of measurements. The Common-Mode Input Capacitance on this part is 8.8pF, which at 10KHz will result in ∼1.8 MOhm impedance, Differential Input Capacitance…