• RE: AD8605 Howland Current Source unstable for bioimpedance

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD8605 application for -25℃, 25℃ and 75℃

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD8605 schematic with ICS-40300 questions?

    Dear All,

    The project is for acquiring heart sound device with MCU ADC. The input frequency range are from 20Hz to 2KHz.

    For lower frequency performance, a high SPL analog microphone is selected. We also saw some documents about microphone preamp circuit…

  • About AD8605 Offset Voltage Temperature dependence Condition

    I have Qustion about AD8605 Offset Voltage Temperature dependence Condition.

    The detasheet P4 say 

    Offset Voltage
    VOS : −40°C < TA < +125°C MAX 750 μV

    The condition is only Vcm=Vs/2 or Vcm 0 to 5V ?

  • AD8605 EMI immunity

    The system might be affect by strong EMI.

    Depending on the test of 120MHz 1dBm, AD8605 output is wrong.

    Of course the customer takes case about pattern layout. they put 1Mohm resistor near the pin.

    But the issue is not cleared.

    Can the customer put…

  • AD8605 的供电问题

    为什么AD8605  AD8606 的datasheet 上写的是单电源供地 (2.7V~5.5V),但是 ADI 的 应用笔记(CN0272)上AD8605的供地确实±5V呢?? 到底是是单电源供地还是双电源供电???双电源供电不会坏掉吗??

  • 请问使用AD8605轨到轨放大器时,如下互阻放大器电路能否正常工作?

    请问轨到轨放大器同相输入端和光电探测器正端可以接地吗?还是要接一个偏置。

  • AD8605 AD8608的外围电路该如何设计(光电二极管前置放大器)

    想使用AD8605 ad8608 进行光电光电二极管前置放大器的设计 它的外围电路该如何设计 比如 Cf Rf 还有输出端滤波等等 有没有相关的参考设计和说明文档 谢谢

  • Can I use AD8605 with -3.3V: connect ground to V- and -3.3V to V+ to get negative outputs?

    I want to use it to have a negative voltage for the EAM bias voltage.

  • 我用AD8605运放可是放大倍数跟我计算不一样。

    我根据此图做的运放,可是放大倍数确是5倍多是怎么回事呢。应该是十倍才对