• AD8605 SPICE Model Input Capacitance

    AD8605 Specifies CCOM as 8.8pF and CDIFF as 2.6pF yet the SPICE model defines only:

    C1 14 16 0.6E-12
    C2 17 18 0.6E-12

    which I think are the CCOM values. In order to simulate these correctly, is it best to simply add the components externally.

    Many…

  • Unexpected AD8605 filter behavior in LTspice

    I'm using LTspice to simulate a LPF using the AD8605. I'm expecting this circuit to attenuate high frequency signals but the output I'm getting is attenuation at any frequency, more so at low frequencies. As a sanity check I've made sure I have…

  • AD8605

    Can this be used as a comparator? and how? Thanks

  • how to test the AD8605 as TIA (I to V) design using current source?

    Hello,

    I am trying to test the Trans-impedance amplifier design using AD8605 for the photo-diode application circuit.

    currently i am using an NI 9265 module to generate current source up to 20mA in my setup 

    below is my circuit:

     

    when i try to set the…

  • AD8605如何用于protelDXP 2004

    需要利用AD8605在protelDXP搭建模型,并且建立相应的PCB板图,但是protelDXP中没有AD8605的模型,如何获得可以运用于protelDXP的模型,即元件。

  • AD8605

    Hello, is AD8605 a current-feedback op amp? I couldn't find this information on data sheet.

    Thank you.

  • AD8605 input protection

    Hi,

    Does the AD8605 have a protection against voltages below 0V ?

    I can see in the datasheet (p 16) that there is a protection against overvoltage. It says that if the voltage is 0.5V higher than Vcc supply, a current limiting resistor should be added…

  • AD8605 4 level filter can't work

    Hello, I design a 4 level filter in accordance with the online design wizard of ADI, as follows, but, it finds that the second level is output 0V. Why?  how to adjust and test?

    U1:AD8605;

    Single power supply 4V;

    VREF = 2V;

    The first stage output 5mV…

  • RE: AD8605 performances at -55°C

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,