• AGC problem on LTspice with AD8330 and LTC5507

    I'm trying to simulate an AGC circuit employing AD8330 as VGA, LTC5507 as power detector and AD8601 as a general OPA in the feedback loop, as in the attached schematic. I'm finding the same simulation problem that I had when I was testing the AD8330 VGA…

  • RE: Driving analog data convertor AD7823 with an op-amp

    First of all, thanks for all the responses.

    I'm interested in amplifying a positive signal (between 0-50mv) from a similar photoreceiver to this one and would like to be able to utilize as much as I can of the AD7823 resolution with only a single…

  • Noise analysis ADIsimPE

    Original Question: Noise analysis by Tarzan

    Hi there,

     

    I just started using ADISIMPE recently and I have a question about noise analysis.

    I tried to check output/input noise of the amp circuit.

    But the result of the graph is pretty wired.

    The output…

  • RE: 专家经验分享:宽动态范围的高端电流检测的三种解决方案

    解决方案二:利用AD8210 和外部器件进行高端电流检测

    图2a 所示为集成高压双向分流监控器AD8210 的简化框图;图2b 所示为采用外部基准电压源的单向应用。

    图2. (a) 高压双向分流监控器AD8210;(b) 采用外部基准电压源的宽范围单向应用

    AD8210 可以放大正或负电流流过分流电阻时产生的小差分输入电压,同时抑制高共模电压(最高65 V),并提供以地为参考的缓冲输出。

    如图2a 所示,它主要包括两个模块:一个差分放大器和一个仪表放大器。输入端通过R1 和R2 连接到差分放大器A1…

  • RE: ADI应用解决方案全接触——锂电池管理

    通常,小型/中型混合动力汽车所需的电池电压在60 V200 V之间。镍氢电池在这些电压和能量级别上有一定的优势。然而,完全混合/插电式混合动力或纯电动汽车通常需要300 V以上的电池组,锂电池正是理想之选。 据业界市场咨询公司的公开数据显示,目前锂电池电动车的市场份额在2.5%左右,预计三年之内将达到20%。

    48V及以下电压的锂电池单元在微混动汽车和工业储能中的应用率很高。系统由1315个锂电池单体构成。由于锂电池固有特性,需要对该数量的电池单体进行精确监测,以保障系统安全性并提高电池效率和寿命…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • 专家经验分享:宽动态范围的高端电流检测的三种解决方案

    专家经验分享:宽动态范围的高端电流检测的三种解决方案 by ADI_Amy

    在电机控制、电磁阀控制、通信基础设施和电源管理等诸多应 用中,电流检测是精密闭环控制所必需的关键功能。如何设计宽动态范围的高端电流检测电路,这对于大多数工程师来说都具有挑战性,这里分享由ADI技术专家Neil Zhao、Wenshuai Liao 和Henri Sino提供的几个建议电路供大家参考。

    将按照设计复杂度从高到低的顺序介绍三种可选解决方案,它们能针对各种不同的应用提供可行的高精度、高分辨率电流检测。
    1. 使用运算放大器…