May i use the AD8597 powered from a single supply +5V/GND (input = output = 2.5V DC voltage ref) ?
Because it is only specified with symetrical power (±15V and ±5V).
Is there any drawback for powering any AOP specified for symetrical power, with a single…
LT1028 will work if the circuit has a noise gain of 2 or more. LT1007 is also worth a try; it has higher voltage noise but lower current noise (and pin 5 is open, not boost). Also perhaps AD8597 (with pins 1, 5, and 8 open). ADA4898-1 and ADA4004-1 are…
请提供IC AD8597ARZ的spice模型。是否可以使用AD8599的SPICE模型来仿真AD8597?
AD8597和AD8599数据手册(第6页至第14页)所示的典型工作特性不相同。因此,我认为不能将AD8599模型用于AD8597。请确认并提供AD8597的模型。
Thank you for the feedback, LLoben !
The application basically is scanning with a step frequency of 200kHz. The settlement time of the stimulus (input of the photodiode) is pretty fast (<300ns). For the photodiode/TIA side simulation/calculation based…
Dear Harry,
Sorry for the late answer and thank you for your response.
You are right, the input voltage noise of the AD797 can go up to 1.2nV/sqrt(Hz) and no more than 1.15nV/sqrt(Hz) for the AD8597. So I have to order a lot of components today, I will…
AD8692用AD8691的spice模型,AD8692是双运放,AD8691是单运放。
其他器件如果在LTspice中找不到,可以到ADI官网上下载相关spice模型(.cir文件),每一个运放的页面基本都能找到相关的spice模型(一般在Datasheet下面)。然后将cir文件导入到LTspice中自建电路模型。
附件中是如何在LTspice中导入模型文件的方法:PDF
Hi Jordyn,
Thanks for your reply.
I have reconfirmed and the measurement range is 70mV max. My people have
refused to give details of Thermocouple but they mentioned that it is
chromel -alumel type.
I also saw the table you have mentioned. but I…