• Can I supply the AD8572 with sources ±5.0 V? 

    Hello,

    My question is if I can supply the AD8572 with positive sources 5v (pin V+) and negative voltage 5v (pin V-).

    Thanks,

    akarko01

  • RE: 想找一个偏置电流和偏置电压都小的运放,求推荐

    可以考虑一下 AD8554 AD8551 AD8572 AD8571

    如果要求偏流小,推荐AD549

    如果要求offset 小,推荐ADA4528-1/-2

  • RE: 有奖分享——最爱ADI放大器

    我最近使用的ADI的运算放大器为:ad8572具体特征如下:

    低失调电压:1 µV

    5 V/2.7 V单电源供电

    高增益:145 dB(典型值)

    共模抑制比:140 dB(典型值)

    电源抑制比:130 dB(典型值)

    能够实现轨道贵输出

  • 单级运放放大直流信号的放大倍数可以放大到1000倍么

    请假各位老师。AD8572运放,用于放大一百多mv缓慢变化的直流信号,可以将单级运放的放大倍数加大到1000倍么;

    因为基本是直流信号,增益带宽积肯定应该是可以满足了,不知道有没有别的要求和影响

  • RE: What is the Common mode voltage range of ADA4522-2 ?

    Hi Ashok,

    I would follow harry's recommendation regarding the C4 as well as the tolerance and tempco of the R3 since it directly affects the accuracy of your current source.

    I checked the AD8572 and it is also up to 5.5V supply voltage only. Its…

  • AD822: Phase reversal

    Tha datasheet states that the opamp AD822 do not phase invert the output signal
    when the input signal exceeds the supply voltage, but it does. How can that be?

     

    It is important to distinguish between over-voltage protection (i.e. the
  • AD8628: Signal sourcing

    Reading the 8628 data sheet I don't see the simplified block diagram of the
    amplifier. The question is the following: when looking to the signal source
    trough AD8628 is that mean that 8628 connected to the signal source only half
  • AD7173-8 and multiple channel sampling

    Hi everyone, I am trying to use AD7173-8 in an application where 3 channels are to be used and I am a little confused about that.

    In particular:

    • The AD7173-8 is connected to a microcontroller via SPI. I have configured SPI according to the datasheet…
  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • RE: 印象•ADI放大器——有奖互动,说出你的ADI放大器印象

         对于学工科的学生来说是一个耳熟能详的词。运算放大器作为最通用的模拟器件,广泛运用于信号变换调理、ADC采样前端和电源电路等场合。大家在学习模电课程的时候,都已经学会了运放的设计。然而在使用运放的时候,又有哪些需要注意的呢?

    1、注意输入电压是否超限

         图1-1是ADI的OP07数据表中的输入电气特性的一部分,可以看到在电源电压±15V的条件下,输入电压的范围是±13.5V,如果输入电压超出范围,那么运放就会工作不正常,出现一些意料不到的情况。

    2、不要在运放输出直接并接电容

    在直流信号放大电路中…