• RE: AD8554 - Gain Bandwidth Product doesn't depend on Gain

    Andre,

      Consider it as a summing amp and calculate the noise gain with R6 at min and max.

    BTW, The AD8554 is a first generation AZ part.  I would use the AD8630.

    Harry


  • AD8551 / AD8552 / AD8554: typo in datasheet Rev D figure 68

    In figure 68 of AD8551 / AD8552 / AD8554 datasheet Rev D the part shown part in
    the circuit is AD8552 and not AD8551. This is the conclusion of comparing the
    figure with the pin configuration on page 1. The part in the circuit should be
  • RE: 想找一个偏置电流和偏置电压都小的运放,求推荐

    可以考虑一下 AD8554 AD8551 AD8572 AD8571

    如果要求偏流小,推荐AD549

    如果要求offset 小,推荐ADA4528-1/-2

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • 最爱ADI放大器-ADA4817

         其实用过ADI的IC还是比较多的,没办法一一列出来,就说几个最近在用的,比如基准电压ADR361,ADR360,ADR440,ADR127等等,还有各种放大器,RRIO的精密运放AD8554,低Ib,高带宽,高压摆的电压反馈型ADA4817,超低输入偏置电流的AD549,用来做皮安表非常棒,也是超爱,还有其它一些年代比较久远忘记全名了,也懒得去查。

         现在说说我最爱的ADA4817,它的最大特点就是高带宽高压摆并且拥有超低输入偏置电流,带宽上G,压摆印象中是800V/us左右,输入偏置电流是pA级别的…

  • RE: 印象•ADI放大器——有奖互动,说出你的ADI放大器印象

         对于学工科的学生来说是一个耳熟能详的词。运算放大器作为最通用的模拟器件,广泛运用于信号变换调理、ADC采样前端和电源电路等场合。大家在学习模电课程的时候,都已经学会了运放的设计。然而在使用运放的时候,又有哪些需要注意的呢?

    1、注意输入电压是否超限

         图1-1是ADI的OP07数据表中的输入电气特性的一部分,可以看到在电源电压±15V的条件下,输入电压的范围是±13.5V,如果输入电压超出范围,那么运放就会工作不正常,出现一些意料不到的情况。

    2、不要在运放输出直接并接电容

    在直流信号放大电路中…