• AD8546 'resistive load' limits

    Recently I needed to specify a dual opamp with uncritical specs, for use in an oven controller:

    (The other half of the amp interfaces the thermistor to the ADC, not shown.) 

    A quick parametric search suggested that the AD8546 would be a good fit. Now…

  • RE: 发帖就送话费啦(限前一百名哦),还有大奖等您拿(获奖名单已公布)

    继今年1月ADI中国官网正式推出在线购买平台之后,该公司日前又携手e络盟推出小批量团购优惠活动。在此次为期半年(截止7月31日)的活动中,ADI提供了86款精选放大器产品,包括详细的硬件、软件、电路图、产品材料清单(BOM)等信息,并以千片的优惠价格在e络盟网站上发售。ADI方面承诺上述86款产品不再有最小订货量的限制,即使只买一片,也可以享受和ADI官方一致的千片报价。 从2011年推出参考电路,到2013年推出参考设计,再到2014年推出小批量团购优惠活动,ADI对中小客户的扶持力度正在得到逐年的加强与落实…

  • Comment on 【在线研讨会回顾】放大、电平搬移和驱动精密系统

    会后咱们的专家,放大器应用工程师David对大家各种问题给出了详细的解答,我们选出了其中具有代表性的问题,整理分享给大家。


    【问】

    轨到轨是什么意思?

    【答】

    轨到轨输出放大器是指输出可以非常接近电源轨,比如单电源5V供电时,输出可以非常接近0V或5V,但有多接近还与负载需要的电流有关。

    【问】

    请问使用仪表运放,如何降低1/F噪声?

  • RE: 工程师百问百答——放大、电平搬移和驱动精密系统

     

    【问】

    轨到轨是什么意思?

    【答】

    轨到轨输出放大器是指输出可以非常接近电源轨,比如单电源5V供电时,输出可以非常接近0V或5V,但有多接近还与负载需要的电流有关。

    【问】

    请问使用仪表运放,如何降低1/F噪声?

    【答】

    1/f噪声是放大器固有的,如果要求高,可以在外加fc较低的低通滤波器对噪声进行滤除,但有源低通滤波器也会引入额外的噪声…

  • What amplifier would you recommend for a low power  4mA to 20 mA  current loop transmitter application?

    For low power application that requires RRIO and greater than 5V supply, I would recommend the AD8657 due to its low supply current of 22 uA per amplifier. The AD8657 is a 18V, micropower, rail-to-rail RRIO amplifier optimized for low power and wide operating…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • ADI运算放大器选型指南

    ADI运算放大器选型指南