• RE: AD8541 Large Signal Voltage Gain 's Vs dependency

    Dear Anna

    I beleve in ADI datasheet.

    This Avo feature is changed by Vs drastic.

    So I would like to know changing point.

    Regards

    moto

    Dear Anna Datasheet say "The AD8541/AD8542/AD8544 are optimized to maintain high gains at lower supply voltages…

  • RE: to connect or not to connect Multiple ADA4930-2 Vocm(x) together

    Hi Ching,

    You can actually use any op amps as a buffer but I would recommend AD8542, ADA4001-2, or AD8672 because these are low noise, low input bias current op amps that suit your application.

    Also, since you need only two buffers (one for each AD9681…

  • DC voltage divider for the ADALM1000

    The ADALM1000 can do one thing very well - convert an analog voltage to a digital representation. The 16 bit Analog-to-Digital Converter (ADC) in the ALM1000 signal chain has been designed and optimized for a single voltage range, 0 to +5V. So how can…

  • Conditioning ADMP404 output for ADC

    I am looking into using the ADMP404 MEMS mic as a source for medium quality (100-3,000Hz) voice.  Everything runs off a low power 3v supply.  I need to compress/condition the audio input and also amplify it so that it can be digitized using a 12 bit ADC…

  • RE: Transimpedance Amplifier (Photodiode interface)

    What is wrong with it(AD8541, AD8542) being CMOS?  The datasheet says it can run from a single supply as low as 2.7V.

    Back to the subject of spinning a board that will happen on Wednesday.  I just want to get as much worked out as possible before then…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • ADALM1000 interfaced to a DDS Programmable Waveform Generator

    The ADALM1000 has 4 general purpose digital input/output pins which we can use as a serial port, as we saw in this last blog entry. We can use these pins to interface to direct digital synthesis (DDS) waveform generators such as the AD9837, AD9833 and…

  • 重磅推荐!ADI 体外化学分析仪解决方案

    最新解决方案已上线,点击:http://h.analog.com/CN-VC-ANALYZER-ff?ADICID=SOME_CN_P114971 下载完整文档

    体外化学分析仪的典型架构

    生命科学与医疗仪器仪表包括各种不同的系统,比如体外化学 分析仪、流式细胞分析仪、输液泵、透析设备、呼吸器、导管 等设备。体外化学分析仪利用许多电化学和光学技术来分析血 液、尿液、脑脊髓液和其他生物学样本。其中使用最广泛的技 术是光学测量,实例包括比色、吸收、光谱测定和荧光检测方 法。可通过这些方式测量体液中的抗原…