• RE: AD8529, about open-loop gain model

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • 咨询AD8529开环增益模型相关问题

    ADI技术专家

    您好。我在使用AD8529设计一个同向放大电路,其后将驱动电容性负载,因此希望获得AD8529的开环增益模型来预计系统瞬态响应性能并添加适当的补偿。测试方法参照《基于运算放大器和模拟集成电路的电路设计》第3版315页图8.5环路增益的测试(取消掉反向输入端寄生电容和负载电容,此时beta=0.5且无零极点),认为T/beta即为开环增益,测试电路和测试结果详见附件文档。具体问题如下:

    1、使用+5V和-5V供电时,可获得与数据手册基本一致的开环增益曲线;使用+12V和0V供电时…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…
  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • Is ADP2291 working as expected in the datasheet or its examples are fail?

    Hello Everyone,

    Im working on a battery charger circuit. I set completely the figure-22 and the figure-23 in the datasheet. So more than hundred try and later than weeks. The circuits are not working as expected. This part is important "The circuits are…

  • Noise optimizing AD8599 &&

    Good day,

    I have a task to optimize noise in BW 10Hz - 10kHz.

    Voltage gain shall be around 20..50. OA connected directly to source of signal,

    which has impedance 1kOm DC and 50Om AC. OA connected to middle point of R1/R2 divider,

    where R1 connected…

  • ADI运算放大器选型指南

    ADI运算放大器选型指南

  • ADI芯片辨识、型号查找

    看看截图: