• AD8519 input protection

    Hello,

    I am currently designing an input protection (IEC 61000-4-2. level4) for the analog inputs of our system. We did choose the AD8519ARTZ and AD8137YCP amplifiers for our design, but now having trouble to find the maximum transmission line pulse voltage…

  • AD8519: Can ADI provide partial spice model for testing out-of spec issues

    Can ADI provide a partial SPICE model to cover the following out of spec
    parameters:

    Q1. Input voltages limitations, such as Vdifferential, VCM, Vabsolute (> VCC)
    etc.

    Q2. Output true behavior when violating the limitations of…
  • AD8529, about open-loop gain model

    Hello, everyone

    I'm currently designing a non-inverting amplifier circuit with AD8529. Its gain is 2 and it will drive a capacitive load. I want to aquire the open-loop model of AD8529 in order to estimate its transient response and to design appropriate…

  • 咨询AD8529开环增益模型相关问题

    ADI技术专家

    您好。我在使用AD8529设计一个同向放大电路,其后将驱动电容性负载,因此希望获得AD8529的开环增益模型来预计系统瞬态响应性能并添加适当的补偿。测试方法参照《基于运算放大器和模拟集成电路的电路设计》第3版315页图8.5环路增益的测试(取消掉反向输入端寄生电容和负载电容,此时beta=0.5且无零极点),认为T/beta即为开环增益,测试电路和测试结果详见附件文档。具体问题如下:

    1、使用+5V和-5V供电时,可获得与数据手册基本一致的开环增益曲线;使用+12V和0V供电时…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…
  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • ADI芯片辨识、型号查找

    看看截图:

  • Noise optimizing AD8599 &&

    Good day,

    I have a task to optimize noise in BW 10Hz - 10kHz.

    Voltage gain shall be around 20..50. OA connected directly to source of signal,

    which has impedance 1kOm DC and 50Om AC. OA connected to middle point of R1/R2 divider,

    where R1 connected…

  • 工程师必读的放大器设计100问(ZT)

    网上看到以对答形式总结的基本原理、概念及实用经验,非常棒的资料,转发分享,放大器应用是个经验活,希望大家多分享交流:

    噪声是电子设计中必须处理等信号之一,我们都知道放大器的噪声有两种类型:一种是外部噪声,来源于放大器外部;另一种是内部噪声,来源于器件本身,处理放大器的噪声对于提升电子产品的性能至关重要,这里我们以问答形式对放大器噪声原理进行阐述,并阐述一些如何处理放大器噪声等实用技巧。

    Q1 [问:] 放大器的内部噪音如何进行精确测量?它和那些因素有关?在测试时需要注意那些问题?