• AD8468 spice model

    Hello everybody

    I need spice model of AD8468. Could you please help me?

    Thanks a lot :)

  • Failure probability for AD8468

    I need the FIT (failure in time) or failure per million hours from the AD8468
    part.

     

    If you go to this address:

    http://www.analog.com/en/quality-and-reliability/reliability-data/content/index
    .
    html

    --or--

    go to www…
  • AD8468两个输入端都接地,输出是高电平还是低电平

    AD8468两个输入端都接地,输出是高电平还是低电平

  • RE: AD790 3.3V Logic Supply ?

    Hi Johnny,

    The AD790 datasheet shows that the logic supply range is 4V to 7V... So no, it can't be powered by 3.3V.

    There are other comparable comparators that you can consider, such as the AD8468/ADCMP608.

    Good luck!

    Reemo

  • RE: AD790, temperature considerations

    FormerMember
    FormerMember

    usaghi-san,

    The problem is finding a new part that runs on +/-15V and is in a PDIP;  there aren't any.

    Look at the AD8469, AD8468, ADCMP609 or ADCMP608.  You can get little adaptor boards

    from sparkfun.com and solder SOICs on it and plug it in a…