I have the same problem at the moment
Is there a sample circuit for the cs pin?
I have the same problem at the moment
Is there a sample circuit for the cs pin?
Using AD8450, when the PGIA is tested and set to 0 drift or 20mv, why is the output of PGIA always negative
Why AD8450 compensation design tools, when using the software does not reflect?
Hello,
I am looking forward to using the AD8450 with batteries up to 42V. The Bus voltage would be 48V. Within specs from what I understand.
The 42V with the lowest PGDA gain (0.2) will lead to a worst case loop error of 8.4V, which is over the control…
Hello all,
I am software embedded engineer and I am looking for the software drivers for the AD8452.
Is there already written “Hello World” for this AFE? I suppose, that I need to use an AD8452 and µC ADUC7061. Maybe ADUC7061 and the evaluation boards…
AD8450+ADP1972锂电池充放电,设置锂电池的放电电流为20A时,为什么输出电压会有波动(用负载代替锂电池),ADP1972的SS引脚在开启后它会是一个上升—下降—上升—下降的波形