I want to purchase AD 844 current feed back operational amplifier, I have done simulation of a circuit which involves AD 844. Now I want to design that circuit but I am not sure How to feed current as an input in AD844.
AD844 require current as an input…
我在做电流发生器时,用到AD844 。 TZ管脚与2管脚电流相同,这个相同有什么限制条件??以及2管脚和3管脚电压相等时的条件限制??
I want to purchase AD 844 current feed back operational amplifier, But i am facing a problem while doing simulation part on PSPICE simulator. It is written in data sheet that in case of CFOA current at pin 5 Iz=+ or - of Ix.
With the help of AD 844…
Kind of cruising through the industry CFA datasheets for the better DC error ones for this next PlanetAnalog article - There was more effort than usual in the old AD844 datasheet, which is nice, but I happened to notice looking down a bit further there…
按照上图进行电路搭建后(R=1.5k,电源电压±15V,Uout输出所接RC分别为1.5K和0.1uF),Uin输入8KHz,1.5V的正弦信号,希望输出幅值1mA的正弦恒流源,但实际测试发现,低负载状况下(ZL<5K),线性度较好,当负载大于5K时,实际幅度<ZL*1mA,(10K负载时,实际输出只有9V),为何?理论上不是应该等于ZL*1mA么?analogchina-adminFormerMemberhdx2FormerMemberAnalog1ezchinatest112…
为什么pspice中的AD844只能放大到400mV左右,官网的spice模型也是400mV左右,实际中易震荡了,放大倍数又是提不上去,有没有好的方法来解决这个问题呢,是不符合稳定条件,还是电源耦合,也可能去耦不好,头快炸了,总之是见鬼了,有没有lBOARD LAYOUT参考啊,请教大家,小弟不胜感激
下图是个仿真例子,另外那个过冲怎么回事啊
AD844的第5pin是用来做补偿的,尤其是在驱动容性负载的时候需要添加RC做补偿,保证输出的稳定性。补偿端加220nF的电容可能确实太大了,而且电容接地是否合适呢,另外pin5的电阻接地是有何用意呢?请仔细阅读AD844的datasheet再做电路设计。
we can implement second generation current conveyors with 3 pins of AD844s'. Also i attached the figure of implementation of Differential voltage Current Conevyor with commercialy AD844AN ICs. I want to know about any possible model of Fully deferential…
AD844可以单电源供电吗,我想用他做一个恒流源电路,+5V和地给他供电,没有负电压可以吗
AD817的驱动能力比AD844强,而且AD844驱动大电容性负载需要外接RC,其它特性基本差不多,谢谢回复, !