• AD8366

    ADI的技术大牛们

    你们好

    我最近使用的AD8366的时候出现一个很奇怪的现象,我照着AD8366的datasheet上的P20做了个电路,有几块电路没问题,有两块出现了AD8366的输出端的电压幅度不一样,后来发现输出不一样的AD8366的OFSA和OFSB的对地电容的电压不一样,不知道是输出幅度的不一样导致这两个电容的电压不一样,还是两个电容的电压不一样导致输出幅度的不一样?希望大牛帮我解答一下,并且怎么使两端输出的幅度能保持一致呢?附:Cofs=8200pf。是否控制DENA,DENB这两端都对输出幅度没影响…

  • AD8366 SPI

    AD8366可以使用STM32的SPI进行通讯控制吗?

    有没有相关例程?

  • Driving the AD8366

    Dear Support,

    I am currently designing a frontend for a computer based oscilloscope. The ADC will be the LTC2298 which will be driven by the AD8366.

    The Bandwidth of my Input Signals will be between DC and a few MHz.

    My Question is; Do I need to shift…

  • AD8366: input/output matching networks

    Dear support,

    in my design I would adopt the AD8366 DVGA.

    I want to ask a reference design or some guide lines in order to match the output and input of the AD8366 with the rest of the circuit:

    - on the INPUT the signal is a 50Ohms single-ended.

  • AD8366 Output Common-Mode control

    Hello,

    I am planning to use the AD8366 to drive the dual inputs of the AD9643 ADC. From the AD8366 datasheet, it seems that output common mode voltage is programmable from 1.6 to 3 V only. But by looking at the VCMA equivalent circuit (figure 48 of AD8366…

  • AD8366 output swing compliance with LTC2194

    Dear support.

    In my design I have an AD8366 dual-VGA that drives a LTC2194 dual-ADC.

    Refring  at the specifications for those device, I found the voltage swing of AD8366 is 6Vpp, whereas the absolute maximu ratings for the LTC2194 inputs is 2Vpp.In my…

  • theta-jc of ADL5385, ADL5387, AD8366

    Hello support,

    I need the theta-JC of ADL5385, ADL5387 and AD8366.

    Could you please teach me that ?

    Best regards,

    ysuzuki

  • AD9643 and AD8366 connection in fmcomms1

    Hi,

    As per the schematic of fmcomms1 not all the output of ad8366 amplifier are connected to AD9643 inputs. OPMB and OPPA output of amplifier is connected to the adc via jumper.why the other two outputs of amplifiers are not connected to the adc inputs…

  • AD8366: input/output matching networks (pt.2)

    Dear support,

    Sorry, but I open a new post 'cause it's more then 4 days that I try to reply to my previous question but the forum "reply" option is disabled. I don't know why, but I am wasting lot of time to complete my design. I have also tried to send…

  • AD8366干扰后放大倍数变化

    大家好,AD8366在使用时,当有干扰后,CS脚,SCL,SDA脚同时有脉冲干扰,如下图所示,按理说放大倍数不应变化,但实际中却变化。电路原理图,软件控制图和实际效果图如下,效果图中黄色部分是干扰,蓝色部分是输出信号。