Question: AD8364 is specified to operate up to 2.7 GHz but the datasheet only shows data at 2.5 GHz. Do you have any data showing performance up to 2.7 GHz.
Answer: The attached plots show sweeps of Channel A and Channel B at 2.7 GHz. In the first…
Question: AD8364 is specified to operate up to 2.7 GHz but the datasheet only shows data at 2.5 GHz. Do you have any data showing performance up to 2.7 GHz.
Answer: The attached plots show sweeps of Channel A and Channel B at 2.7 GHz. In the first…
Q.
The AD8364 datasheet provides specification data down to 450 MHz but says that operation down to "Low Frequencies" is possible. Do you have any advice on operating this device below 450 MHz.
------------------------------------------…
I'm developing a microprocessor monitored and controlled RFPA that outputs +30dBm to +61dBm CW between 10MHz to 15MHz. To accomplish this, I need to be able to measure RMS power with at least 40dBm of dynamic range; preferably 50dBm.
There are a number…
尊敬的广大会员及ADI工程师,请教下使用AD8364+ADL5330两器件实现自动增益控制,其响应时间最短为多少us?盼复,谢谢!
I want to measure differential power at different frequencies. I want to use AD8364 detector .How do i calculate power for frequencies whose corresponding slopes are not given in the datasheet?
In the datasheet for AD8364 , there are different max and min input levels for different frequencies .
Are these experimental limits used for calliberation of slope and intercept?
Can i use input power exceeding that given in the datasheet for the frequencies…
The RMS Power Detector AD8364 evaluation board AD8364-EVAL-2140 is described for use at 2140 MHz. To measure 2.4 GHz, will I need to replace the Murata LDB212G1020C-00 balun with the Murata LDB212G4020C-00 myself? Is it possible to make this changes directly…