Q: What is the definition of θJA for paddle soldered/unsoldered shown in the datasheet?
Q: What is the definition of θJA for paddle soldered/unsoldered shown in the datasheet?
Hello,
Do you sell this amplifier as a bare die, without the package?
Thank you in advance,
Hi,
Are ground vias needed on exposed pad?
And if not, is it important to place ground vias as near as possible to the exposed pad?
Indeed the evaluation board doesn't seem to have many ground vias near the exposed pad, which is curious.
Regards
…Hi ,
Device : AD8354
Could you please let me know if you have Gain and Phase margin data with regards to AD8354 .
Thanking you
With best regards and wishes
Hi,
I am trying to receive a 1MHz bandwidth signal with a 1090MHz carrier frequency, since I am not an expert in RF and microwave, i would like to ask you if my current circuit configuration can receive and demodulate the 1090MHz signal using 3 LNAs and…
ADI年度贺岁片——使用AD9851和ADL5350做射频电路的时候的问题 by stevenC
我做过的一个项目中需要用到一些射频器件,其中我使用到的有DDS:AD9851芯片;混频器:ADL5350;RF增益器件:AD8354;自动增益器件:AD8367。大概思路和射频收发器差不错,由DDS产生一个小步进的频率可调的高频信号,用混频器和PLL产生的高频信号混频、滤波后经过放大,驱动功放,在用一个功放期间放大功率后由双工器发送。接收的时候使用到了两次自动增益,然后送入DAC变成数字信号…
AD8353 and AD8354 is specified to operate down to 1 MHz. It can go lower than this. It's just a question of increasing the ac-coupling caps. There is a discussion of this in the apps section of the datasheet along with a plot showing operation down to…
大侠们等辛苦啦,现在公布第二季最强大脑论坛侠士名单~,
恭喜 lbzhuo gongli1991@sina.cn 两位大侠获得“五星侠士”勋章;
恭喜孙治国cnhtzxb@163.comlbzhuo kilua zkf0100007 FormerMemberbati yundong.liu lee@westlakemeter.com yizi0000 wh6ic.99 C_imust momomomo90 liulusong@webmail.hzau.edu.cn 小海不怕 飞翔与思考 en…