• Calculating RF Choke Inductance on AD8353

    For the RF gain block, the AD8353, on page 13 of the datasheet (Rev  C), there is discussion of the need for a RF output choke between the power supply and the RF output when operating at supply levels below 5V. It suggests using a 100 nH inductance for…

  • RE: HMC580ST89 not recommended for new designs

    Hi Jim,

    Your total voltage gain of ~100 corresponds to 40 dB so, each amp in your cascade must provide 20 dB gain.

    For pulses of 5 mV (I'm assuming peak) the second amp in your cascade will need to capable of Pout~=+4 dBm. The only part under RF & Microwave…

  • RE: 求助ADF4360-9与ADL5534的使用及设计方案问题?

    您好!

    建议您先经过变压器将差分信号转为单端信号,然后再进入增益模块,如AD8353。

  • RE: LNA for LORAN

    AD8353 and AD8354 is specified to operate down to 1 MHz. It can go lower than this. It's just a question of increasing the ac-coupling caps. There is a discussion of this in the apps section of the datasheet along with a plot showing operation down to…

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • RE: ADI的RF放大器能不能应用一下范围

    您好!

    ADI工作于2.4GHz频段的射频放大模块产品有很多,请见附件内表格,供您参考。

  • 12/16/2015: Full RF Signal Chains from 0Hz to 110GHz

    Presenter: Mel Conway, Product Manager, Instrumentation, High-speed & RF and Precision

     

    This webcast will explain ADI's new and expanded RF capabilities since the acquisition Hittite Microwave. We will give examples of the wider frequency spectrum…

  • 【在线研讨会讲义PPT下载】从0Hz到110GHz的全频谱RF信号链

    此次在线研讨会阐释了自收购Hittite Microwave后ADI的全新及扩展的RF能力。我们会举例说明ADI涵盖的更宽频谱范围及其真DC的重要性。信号链外的性能同样至关重要,展示低噪声、高稳定性控制和电源元件如何改善总体RF信号性能,并将讨论完整的信号链示例。

    主要讨论天线到比特和比特到天线,信号链覆盖,即刚才提到的从真正的DC 0 Hz到110 GHz的频谱覆盖。 我会简要介绍其中涉及到的各类设备。

    为什么良好的RF需要良好的电源,大家知道,RF需要干净的电源。然后,最后会和大家讨论“不止是芯片…

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF

  • ADI芯片辨识、型号查找

    看看截图: